Festo Media Service

Seleccione una categoría en la columna izquierda o utilice la función de búsqueda.

Pie de foto Download
Un miembro de la familia pequeño pero potente
CMMT-ST El regulador de servoaccionamiento CMMT-ST: el regulador de servoaccionamiento compacto de bajo voltaje para movimientos y posicionamientos de alta rentabilidad. (Foto: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
The right handling system in a matter of minutes
Festo press image of the Handling Guide Online monitor With the Handling Guide Online, machine and equipment manufacturers are able to reduce their time-to-market for integrated handling systems by up to 70%. (photo: Festo AG & Co. KG)
Digitalisation is changing automation in the process industry
Dr. Eckhard Roos Dr. Eckhard Roos, Head of Industry Segment and Key Account Management Process Industries at Festo AG & Co. KG: "Digitisation is moving into the process industry – for example with the Festo Motion Terminal, the first automation platform to be controlled via software apps." (Photo: Festo AG & Co. KG)
Digitalisation is changing automation in the process industry
Motion Terminal VTEM 1 Festo Motion Terminal: fusion of hardware and software to the first valve to be controlled by apps. (Foto: Festo AG & Co. KG)
Digitalisation is changing automation in the process industry
configurator for process valve units Get the right solution quickly and easily with the configurator for process valve units. (Photo: Festo AG & Co. KG)
Moving loads at the tip of two fingers
Festo press photo Balancer Ergonomics improves efficiency – thanks to a servo-pneumatic balancer with the drive solution YHBP from Festo. This enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. (Photo: Festo AG & Co. KG)
Moving loads at the tip of two fingers
Festo press photo balancer system and components Ingredients of the balancer servopneumatic system: pneumatic ISO cylinder, displacement encoder, optionally with safety relay, balancer valve unit VPCB, handle, balancer controller CECC-D-BA with balancer software with browser-based web visualisation. (Photo: Festo AG & Co. KG)
Gestión de datos integral
CPX-E 1 CPX-E es una plataforma integral y unificada de Festo para combinar la técnica de servomotor y de motor paso a paso en funcionamiento mixto (Foto: Festo AG & Co. KG)
Gestión de datos integral
CPX-E 2 Además de ofrecer un gran número de funciones PLC y de tener aplicaciones de múltiples ejes con interpolación, CPX-E puede integrarse fácilmente en sistemas host existentes (Foto: Festo AG & Co. KG)
Un aprovechamiento del espacio sorprendente
ELGC Relación perfecta entre espacio de montaje y espacio operative: el eje accionado por husillo ELGC con servomotor EMME-AS. (Foto: Festo AG & Co. KG)
Un aprovechamiento del espacio sorprendente
EGSC Brilla con dimensiones compactas: mini carro EGSC con servomotor EMME-AS. (Foto: Festo AG & Co. KG)
Astonishing space efficiency
ELGC Ideal ratio of installation to working space: the spindle axis ELGC-BS combined with the servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
EGSC Impresses with compact dimensions: mini-slide EGSC with servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
handling ELGC + EGSC Verblüffende Raumeffizienz: ELGC und EGSC kombiniert in einem Handling-System in adapterfreier „One-size-down“-Montage (eine Größe kleiner möglich) (Foto: Festo AG & Co. KG)
Moving loads at the tip of two fingers
Balancer Ergonomics improves efficiency – thanks to a servo-pneumatic balancer with the drive solution YHBP from Festo. This enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. (Photo: Festo AG & Co. KG)
Moving loads at the tip of two fingers
Balancer system and components Ingredients of the balancer servopneumatic system: pneumatic ISO cylinder, displacement encoder, optionally with safety relay, balancer valve unit VPCB, handle, balancer controller CECC-D-BA with balancer software with browser-based web visualisation. (Photo: Festo AG & Co. KG)
El grupo Festo
Head Office Sede central de Festo en Esslingen a.N., Alemania. (Fotografía: Festo AG & Co. KG)
El grupo Festo
process automation Festo ofrece apoyo a sus clientes en todas las fases del proyecto, desde la ingeniería hasta la puesta en marcha y el mantenimiento. (Fotografía: Festo AG & Co. KG)
El grupo Festo
CP_Factory Cualificación para la Industria 4.0: Festo Didactic ofrece con CP Factory una plataforma física y virtual de aprendizaje e investigación. Esta plataforma reproduce mediante modelos las estaciones de un equipo de producción real. (Fotografía: Festo Didactic SE
First turnkey IoT solution
CPX-IoT-Gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
Portrait Michael Hoffmeister “Festo is working closely with other companies in the German Electrical and Electronic Manufacturers’ Association and on the Platform Industry 4.0 project to create a common reference architecture,” explains Dr Michael Hoffmeister, Management Expert at Festo in the newly founded Digital Business section. (Photos: Festo AG & Co. KG)
First turnkey IoT solution
YXMx Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the modular positioning platform YXMx from Festo. (Photos: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Multi-Carrier-System® 3 Multi-Carrier-System®: el sistema de transporte modular y flexible se puede adaptar por software a distintos formatos con tan solo tocar un botón. (Foto: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Sistema circular Multi-Carrier-System®: el sistema de transporte modular y flexible se puede adaptar por software a distintos formatos con tan solo tocar un botón. (Foto: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Motion Terminal VTEM 3 Festo Motion Terminal es el primer sistema que permite controlar funciones neumáticas con una aplicación, sin necesidad de sustituir o modificar el hardware. (Foto: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Motion Terminal VTEM 2 Festo Motion Terminal es el primer sistema que permite controlar funciones neumáticas con una aplicación, sin necesidad de sustituir o modificar el hardware. (Foto: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Sistema completo VTEM y MCS Cambio de formato simplemente pulsando una tecla: dos innovaciones de Festo permiten cambios de formato sencillos y que solo haya que realizar en una máquina – Festo Motion Terminal VTEM y Multi-Carrier-System® MCS. (Foto: Festo AG & Co. KG)
Cambio de formato simplemente pulsando una tecla
Sistema de pinza Flexibilidad máxima: Los envases de distintos tamaños y el número correspondiente de productos se colocan directamente en Multi-Carrier System® (MCS) mediante los carros (portadores) de libre posicionamiento. Este procedimiento permite transportar en el carro, agrupar y empaquetar de forma sincronizada los productos. (Foto: Festo AG & Co. KG)
30 mostrar otros resultados ...