2018-11-27

Cycle times reduced by 30 per cent

Cycle times reduced by 30 per cent

Cantilever axis ELCC-TB with low moving mass
The cantilever axis ELCC-TB is an important part of Festo's philosophy of complete connectivity.

Compact design for 30% shorter cycle times and 50% less vibration – those are the most important characteristics of the cantilever axis with toothed belt ELCC-TB from Festo. The axis fits in seamlessly with Festo's concept of complete connectivity for its electric automation technology.

 

The high rigidity of the toothed belt cantilever axis cuts vibrations in half, whilst the low moving mass of the compact design reduces cycle times by almost a third. A stainless steel cover strip protects the internal recirculating ball bearing guide. Thanks to sealing air, the cantilever axis ELCC-TB is suitable for use in dusty environments or on machine tools. A clamping unit securely holds loads and acts as an emergency brake.

 

With a stroke of up to two metres, the cantilever axis is ideally installed vertically as a Z-axis, for example for palletising or erecting boxes. It can also be used horizontally or at any other installation angle if the axis has to be removed from the working space.

 

Complete connectivity

The cantilever axis ELCC-TB is an important part of Festo's philosophy of complete connectivity, i.e., the ability to connect a workpiece completely through to the cloud, from its mechanical connections and electrical interfaces to commissioning and controller programming. This simplifies the work of every machine builder and automation engineer when it comes to connecting the mechanical and electric technology as well as the control levels and their interfaces with the hardware and software.

 

Contact:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo Media Service

 
 

Photos

Caption Download
ELCC Cantilever axis ELCC in size 90 for vertical or horizontal operation. (Photo: Festo AG & Co. KG)
ELCC cardbox application Cantilever axis ELCC for erecting cardboxes. (Photo: Festo AG & Co. KG)