Festo Media Service

Please select a category on the left or use the search.

Caption Download
Pneumatic robotics meets artificial intelligence
BionicSoftHand 1 The BionicSoftHand should rotate a 12-sided “cube” so that a previously defined side points upwards at the end.
Pneumatic robotics meets artificial intelligence
BionicSoftHand 2 The BionicSoftHand is operated pneumatically for the safe and direct interaction with people.
Pneumatic robotics meets artificial intelligence
BionicSoftArm 1 The pneumatic lightweight robot BionicSoftArm is flexible from the start and is suitable for direct human-robot collaboration.
Pneumatic robotics meets artificial intelligence
BionicSoftArm_SCARA The BionicSoftArm as a classic SCARA application with a pick-and-place task: it can work in the tightest of spaces around obstacles.
Digital Maintenance Management by App
Smartenance Smartenance: the first digital maintenance app for system operators and production managers. (Photo: Festo AG & Co. KG)
Condition monitoring in the cloud at the press of a button
Dashboard Improves operating transparency for production managers and operators: turnkey, preconfigured dashboards of Festo. (Photo: Festo AG & Co. KG)
Adding value to supply chains through additive manufacturing
Festo press photo HP Center of Excellence 1 HP’s new 150,000 sq. Ft 3D Printing and Digital Manufacturing Center of Excellence in Barcelona, Spain. (Photo: HP)
Adding value to supply chains through additive manufacturing
Festo press photo HP Center of Excellence 2 HP’s new facility integrates flexible layouts for collaboration across engineering, R&D groups, customers, and partners with fleets of the latest plastics and metals 3D production system for rapid and agile product development. (Photo: HP)
Bringing artificial intelligence directly to the machine
Festo press photo Tanja Maaß “The crucial factor is therefore bringing AI directly to the machine and interpreting data there – directly at the source – in real time”, says Tanja Maaß, Resolto’s Managing Director. (Photo: Resolto Informatik GmbH)
Bringing artificial intelligence directly to the machine
Festo press photo Resolto The Scraitec software solution from Resolto knows the healthy condition of a plant and detects every anomaly with the real-time analysis of the plant’s sensor data. (Photo: Resolto Informatik GmbH)
Bringing artificial intelligence directly to the machine
Festo press photo CPX-IOT With the Festo IoT Gateway CPX-IOT as hardware, customers can have their machine and plants monitored at field level. Field level support is provided with the ScraiField software component. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Dr Michael Hoffmeister “Getting started couldn’t be easier: Festo has a host of digital products from which users can already benefit”, explains Dr. Michael Hoffmeister, Executive Expert Digital Business with Festo. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Smartenance Smartenance: This software program from Festo is a digital maintenance manager for production managers and plant operators, available for download as an app. (Photo: Festo AG & Co. KG)
How will the digitalisation of mechanical engineering evolve?
Plattform Industrie 4.0 Plattform Industrie 4.0, the digitalisation initiative of the Federal Republic of Germany: Since 2018 Festo has – in the person of Chief Technology Officer Dr. Frank Melzer (right) – held the chair of the platform’s steering committee. (Photo: Festo AG & Co. KG)
Innovation pays off
Festo press photo, 2019 DMG MORI Innovation Partner Award Festo was presented with the DMG MORI Innovation Partner Award 2019 at the EMO. From left to right: Christian Thönes, Chairman of the Management Board at DMG MORI AKTIENGESELLSCHAFT, Timo Rickermann, Chief Purchasing Officer at DMG MORI AKTIENGESELLSCHAFT, Dietfried Lustig, Global Key Account Manager at Festo, Dr. Oliver Jung, Chairman of the Management Board at Festo AG, moderators Angela Julie Wadenpohl and Yasmine Blair, as well as Dr.-Ing. Masahiko Mori, President of DMG MORI COMPANY LIMITED. (Photo: DMG MORI)
Move loads of up to 999 kg at the touch of a finger
Balancer Ergonomics improves efficiency: a servo-pneumatic balancer combined with Festo's drive solution YHBP allows employees in assembly and logistics to lift and move loads effortlessly, at the touch of a finger. (Photo: Festo AG & Co. KG)
Move loads of up to 999 kg at the touch of a finger
Kia door fitting Kia Motors Slovakia counts on the balancer for fitting doors in its vehicle production. (Photo: Kia Motors Slovakia)
Move loads of up to 999 kg at the touch of a finger
Kia wheel fitting The balancer’s ergonomic benefits also come into their own when fitting wheels in Kia Motors’ car production plant in Slovakia. (Photo: Kia Motors Slovakia)
25 per cent less power consumption
PreAudit 1 The PreAudit gives an overview of the entire compressed air system, from the compressor to the pneumatic application. (Photo: Festo AG & Co. KG)
25 per cent less power consumption
PreAudit 2 The compressed air experts from Festo uncover significant potential for savings, for example by measuring the pressure loss. (Photo: Festo AG & Co. KG)
25 per cent less power consumption
PreAudit 3 Documented results provide advice and recommendations for energy efficiency. (Photo: Festo AG & Co. KG)
BionicCobot could revolutionise the textile industry
BionicWorkplace 1 Exciting concept study from Festo: in the BionicWorkplace, a person works with a robot arm as well as numerous assistance systems that are networked with each other. (Photo: Festo AG & Co. KG)
BionicCobot could revolutionise the textile industry
BionicWorkplace 2 The future in sight: a worker can intuitively control the BionicCobot using movement, touch or speech. (Photo: Festo AG & Co. KG)
BionicCobot could revolutionise the textile industry
BionicWorkplace 3 The future belongs to sensor technology. Sensors and camera systems record the positions of the worker, components and tools. (Photo: Festo AG & Co. KG)
인공 지능형 공압 로봇
BionicSoftHand 1 특히 BionicSoftHand는 12면 큐브를 회전시켜 이전에 설정된 면의 끝 부분을 위쪽으로 향하도록 한다.
인공 지능형 공압 로봇
BionicSoftHand 2 BionicSoftHand는 공압으로 작동되므로 사람과 안전하고 직접 상호 작용할 수 있다.
인공 지능형 공압 로봇
BionicSoftArm 1 공압 경량 로봇인 BionicSoftArm은 미래 지향형 컨셉인 인간 - 로봇 협업에 적합하다.
인공 지능형 공압 로봇
BionicSoftArm 2 인간과 로봇의 직접적인 협업은 BionicSoftArm과 픽 앤 플레이스 (pick-and-place) 작업과 같은 고전적인 SCARA 어플리케이션에서의 적용이 가능하다.
인공 지능형 공압 로봇
BionicFinWave 1 실리콘으로 만들어진 두 개의 측면 핀은 별도의 지지 요소가 필요하지 않다.
인공 지능형 공압 로봇
BionicFinWave 2 수중 로봇은 아크릴 유리로 만든 파이프 시스템을 통해 독립적으로 움직인다.
인공 지능형 공압 로봇
BionicFinWave 3 수중 로봇은 아크릴 유리로 만든 파이프 시스템을 통해 독립적으로 움직인다.
Show 30 more results ...