Festo Media Service

Please select a category on the left or use the search.

Caption Download
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
Together at the forefront of robotic milking technology
Lely Press Image Martijn Boelens “Just like Lely, Festo is an internationally active family-owned company which focuses on long-term responsibility instead of short-term profits. When it comes to product development we have a similar approach,” stresses Martijn Boelens, Vice President Customer Solutions at Lely. (Photo: Lely)
Together at the forefront of robotic milking technology
Festo Press Image Arnoud Nieuwdorp “The movements of the hybrd arm of the milking robot Astronaut A5 motion is gentler, and it’s more energy-efficient and faster,” says Arnoud Nieuwdorp, Global Key Account Manager, Festo Netherlands. (Photo: Festo AG & Co. KG)
Together at the forefront of robotic milking technology
Festo Press Image Jan Bredau “With the new robot arm operating and maintenance costs, and thus total cost of ownership, decline as well,” adds Dr. Jan Bredau, head of Systems Engineering at Festo corporate headquarters in Esslingen, Germany. (Photo: Festo AG & Co. KG)
Together at the forefront of robotic milking technology
Lely Press Image Lely milking robot Lely’s milking robot Astronaut A5: Automation helps to avoid hard, monotonous work and to increase output. (Photo: Lely)
Together at the forefront of robotic milking technology
Lely Press Image Robot arm Robot arm of Lely’s milking robot Astronaut A5: with electric axes from Festo and corresponding software. (Photo: Lely)
Together at the forefront of robotic milking technology
Festo Press Image ESBF Powerful, fast and precise positioning - the electric cylinder ESBF. High performance with a rating of 17 kilonewtons and a stroke of 1500 mm. (Photo: Festo AG & Co. KG)
Together at the forefront of robotic milking technology
Festo Press Image EMCA 2 Integrated drive EMCA: The brushless DC motors from Festo with absolute position recording, integrated regulator, power electronics, absolute encoders. (Photo: Festo AG & Co. KG)
Measuring and weighing without contact
SupraSensor_1 The SupraSensor exhibit demonstrates the function of a contactless balance, which could be used for example on sterile workbenches in biological or chemical analytics.
Measuring and weighing without contact
SupraSensor_2 Only the weighing pan carrying the item hovers over the table top – without the danger of cross-contamination via the workplace surface or tools.
Flexible interfaces in plant engineering
Festo press photo VZXA Flexible, robust and offering high performance – the angle seat valves VZXA from Festo control media flows quickly and reliably. (Photo: Festo AG & Co. KG)
Flexible interfaces in plant engineering
Safety block Save space and prevent leakages using several angle seat valves type VZXA in a safety block. (Photo: Festo AG & Co. KG)
Astonishing space efficiency
ELGC Ideal ratio of installation to working space: the spindle axis ELGC-BS combined with the servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
EGSC Impresses with compact dimensions: mini-slide EGSC with servo motor EMME-AS (Photo: Festo AG & Co. KG)
Astonishing space efficiency
handling ELGC + EGSC Verblüffende Raumeffizienz: ELGC und EGSC kombiniert in einem Handling-System in adapterfreier „One-size-down“-Montage (eine Größe kleiner möglich) (Foto: Festo AG & Co. KG)
First turnkey IoT solution
CPX-IoT-Gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
Portrait Michael Hoffmeister “Festo is working closely with other companies in the German Electrical and Electronic Manufacturers’ Association and on the Platform Industry 4.0 project to create a common reference architecture,” explains Dr Michael Hoffmeister, Management Expert at Festo in the newly founded Digital Business section. (Photos: Festo AG & Co. KG)
First turnkey IoT solution
YXMx Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the modular positioning platform YXMx from Festo. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Multi-Carrier-System® 3 Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Recirculating conveyor system Multi-Carrier-System®: the flexible modular transport system can be adapted to different formats via software at the push of a button. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Motion Terminal VTEM 3 With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Motion Terminal VTEM 2 With the Festo Motion Terminal, pneumatic functions can be controlled via apps for the first time, without having to change or modify the hardware. (Photos: Festo AG & Co. KG)
Format change at the push of a button
Complete system VTEM and MCS Format change at the push of a button: two Festo innovations enable fast and straightforward format changes on just one machine – the Festo Motion Terminal VTEM and the Multi-Carrier-System® MCS. (Photo: Festo AG & Co. KG)
Format change at the push of a button
Gripper system High flexibility: Different box sizes and the matching number of products are set directly in the Multi-Carrier-System® MCS using the freely positionable carriers. The products can be individually transported, grouped and synchronously packaged on the carriers. (Photo: Festo AG & Co. KG)
Revolution in automation
Revolution in automation
Revolution in automation
Reliable shut-off of smooth media flows
VZQA The pinch valve VZQA: flexible connection options. (Photo: Festo AG & Co. KG)
Show 6 more results ...