13/06/2019

Equip machines and systems with the Stars in Automation

Equip machines and systems with the Stars in Automation

Over 2,200 components from the Festo core product range are now available for immediate delivery worldwide
With the Festo core product range machine builders can realise around 80% of all applications quickly, effortlessly and at attractive prices

Festo is ready for further growth. The company has already doubled its production capacities worldwide over the last two years. The focus of these efforts has been on expanding the Festo core product range in the field of pneumatic and electric automation products. They are the true 'Stars in Automation Technology' – quickly available worldwide, durable and attractively priced.

 

These Stars in Automation include over 2,200 components from every phase of the pneumatic and electrical control chain, from compressed air preparation, valves and cylinders to accessories, such as matching tubing and fittings. With the Festo core product range, machine and system builders can realise around 80% of all applications quickly, effortlessly and at attractive prices, even when large quantities are needed.

 

Fast availability worldwide

Many of the components marked with the star are ready to be shipped just 24 hours after the order is received, while configurable products are ready for delivery within five days. All products in the core product range are available worldwide and with the same level of quality thanks to automated production at various decentralised locations in the core markets of Germany, China and the USA. There are further plants in India, Brazil, Hungary, the Czech Republic, Bulgaria and Switzerland. Distribution is also decentralised thanks to highly automated logistics centres in Germany, China and the USA, so 70% of all customers can be reached within one day.

 

The hallmark of the latest components of the core product range is the collaboration between the design engineers and production planners at Festo. They worked closely together during the development of these products to ensure that the Festo plants can manufacture the components with a high degree of automation. For example, Festo engineers manufactured the yoke and slide for the new mini slide DGST as a single part in order to enable large quantities to be produced efficiently. The developers successfully reduced the number of components by 60% compared with the previous model.

 

Shorter cycle times

This simultaneous engineering approach allowed Festo to reduce cycle times by almost 50% for the DGST or the guided drive DFM. Festo plants can now produce a DFM every minute, for example. Another example is the fully automated production line for the standard valve VUVG, which produces a fully assembled valve every 12 seconds.

 

The paths between the individual production steps are shortened and throughput times are reduced thanks to new organisational methods. These include aligning production and assembly with value streams and the consistent application of Operational Excellence (OPEX) methods, such as Lean Management or Six Sigma. Festo also intends to use these new methods to increase efficiency and productivity at its production, assembly and logistics locations over the coming years.

 

New stars in the world of automation

The accelerated product development process has paved the way for the latest Stars in Automation. The mini slide DGST, for example, is the smallest of its kind and the shortest slide drive on the market. But it is strong when it comes to precision, forces, motion control, durability and reliability.

 

Other new Stars in Automation include the lightweight compact cylinder ADN-S, which is produced almost entirely as one part and can perform small and micro-movements in the smallest of spaces. The regulators and filter regulators of the MS2 series service units are designed for use close to the process directly in the machine and for end-of-arm applications. They are lightweight and compact, but with high flow rates of up to 350 l/min. The tubing/fitting combination PUN-H/QS also ensures reliable compressed air supply in standard applications but also in wet areas and is suitable for use in the food industry too. These are just some of the more than 2,200 products in the Festo core product range that offer quick availability worldwide at attractive prices.

 

www.festo.com/kernprogramm

 

Contact:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo Media Service

 
 

Fotos

Caption Download
Technology plant VUVG assembly line A compact valve every 12 seconds: automated assembly plants with fast retooling times ensure high output volumes for the automation products of the Festo core product range. (Photo: Festo AG & Co. KG)
DGST Precision and high performance with yoke and slide as a single part: mini slide DGST. (Photo: Festo AG & Co. KG)
DFM Sturdy and compact with a range of mounting options: guided drive DFM. (Photo: Festo AG & Co. KG)
VUVG High flow rate with a narrow width: compact valve VUVG. (Photo: Festo AG & Co. KG)
ADN-S Space-saving and precise with numerous mounting options: compact cylinder ADN-S. (Photo: Festo AG & Co. KG)
MS2 Lightweight and powerful for decentralised applications: filter regulator MS2. (Photo: Festo AG & Co. KG)
PUN-H/Q Variety of colours, transparent, highly flexible: tubing/fitting combination PUN-H/Q. (Photo: Festo AG & Co. KG)