Festo Media Service

Please select a category on the left or use the search.

Caption Download
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
Measuring and weighing without contact
SupraSensor_1 The SupraSensor exhibit demonstrates the function of a contactless balance, which could be used for example on sterile workbenches in biological or chemical analytics.
Measuring and weighing without contact
SupraSensor_2 Only the weighing pan carrying the item hovers over the table top – without the danger of cross-contamination via the workplace surface or tools.
The Festo Group
Head Office The corporate head office of Festo at Esslingen a.N., Germany. (Photo: Festo AG & Co. KG)
The Festo Group
Laborautomation Festo develops intelligent, tested subsystems for the automation of liquid media and sample handling applications. The applications involve the use of both electric and pneumatic actuators with motors, controllers and handling systems, as well as grippers, sensors and camera systems. (Photo: Festo AG & Co. KG)
The Festo Group
Medizintechnik In medical technology, the focus is on the efficient open-loop and closed-loop control of medical gases. Proportional valves with piezo technology are often used in both mobile applications and applications involving the treatment of patients at their bedsides. (Photo: Festo AG & Co. KG)
The Festo Group
CP_Factory Qualification for Industry 4.0: Festo Didactic offers a cyber-physical learning and research platform in the form of the CP Factory. This platform models the stations in a real production plant. (Photo: Festo Didactic SE)
The Festo Group
Festo Press Image EHMD The compact rotary gripper module EHMD, which can not only grip but also open sample bottles, is unique on the market so far. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
CPX-IoT-Gateway Secure connection to the Festo Cloud and exclusive access to individual digitalisation: the IoT gateway CPX-IoT. (Photo: Festo AG & Co. KG)
First turnkey IoT solution
Portrait Michael Hoffmeister “Festo is working closely with other companies in the German Electrical and Electronic Manufacturers’ Association and on the Platform Industry 4.0 project to create a common reference architecture,” explains Dr Michael Hoffmeister, Management Expert at Festo in the newly founded Digital Business section. (Photos: Festo AG & Co. KG)
First turnkey IoT solution
YXMx Kinematics with controller, software packages for motion tasks and condition monitoring, and an app for cloud-based visualisation: the modular positioning platform YXMx from Festo. (Photos: Festo AG & Co. KG)
Automation for laboratory samples
Festo press photo Laboratory Platform Precise handling systems handle and transport highly sensitive samples and fluids. (Photo: Festo AG & Co. KG)
Automation for laboratory samples
Festo press photo Scan Module Automated documentation of the samples using a sensor helps to minimise mistakes caused by repetitive work. (Photo: Festo AG & Co. KG)
Automation for laboratory samples
Festo press photo Washer Module Compact functional solutions such as the washer module here facilitate applications in small spaces. (Photo: Festo AG & Co. KG)
Automation for laboratory samples
Festo press photo Planar Surface Gantry Compact design: with the planar surface gantry EXCM, it is the sample vials that move rather than the needles – this reduces the movement of the pipette to a minimum. (Photo: Festo AG & Co. KG)
Automation is the answer to increasing sample numbers
Festo press photo Chart Degree of Automation High flexibility: individual automation concepts adapt to the requirements of the laboratory. (Photo: Festo AG & Co. KG)
Automation is the answer to increasing sample numbers
Festo press photo Laboratory Platform Linear automation links modules within a process. The samples are automatically transported from device to device. (Photo: Festo AG & Co. KG)
Automation is the answer to increasing sample numbers
Festo press photo Scan Module High quality and reproducibility: automated documentation of the samples using a sensor helps to minimise mistakes caused by repetitive work. (Photo: Festo AG & Co. KG)
Automation is the answer to increasing sample numbers
Festo Pressebild Kleinbauendes Handlingsystem Integrierte Automationslösung: Innerhalb eines Gesamtsystems lassen sich komplette Prozesse und Ergebnisse leichter nachvollziehen und rückverfolgen. (Foto: Festo AG & Co. KG)
DNA extraction now with high throughput
Festo press photo LGC 1 Fully-automatic extraction of DNA becomes almost as easy as child's play: thanks to the oKtopureTM from LGC. (Photo: Festo AG & Co. KG)
DNA extraction now with high throughput
Festo press photo LGC 2 The high level of automation is provided by a handling system from Festo, whose experts in the production of pneumatic and electric automation technology adapted this precisely to the requirements of the customer's laboratory application. (Photo: Festo AG & Co. KG)
DNA extraction now with high throughput
Festo press photo LGC 3 Dr Dietrich Koester "The fact that Festo could offer us a complete package consisting of hardware, software and a consultancy service is what tipped the balance in their favour," explains Dr. Dietrich Köster, Product Manager with LGC. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
Festo press photo Dr. Frank Jacob "Festo develops components and system solutions which will allow laboratories and the manufacturers of medical equipment in future to operate even more productively, reliably and cost-effectively," reports Dr. Frank Jacob, Head of Business Area Medical Technology and Laboratory Automation at Festo. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
Festo press photo respiration 1 CPAP (Continuous Positive Airway Pressure) respiration combines patients' spontaneous breathing with a constant controlled overpressure. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
Festo press photo eye surgery 1 The surgical tools used in ophthalmological operations are pneumatically driven. Solenoid and piezo valves regulate pressure and vacuum, working with various liquids and gases. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
Festo press photo eye surgery 2 The pneumatic control unit is responsible for the following functions: pneumatic drive of surgical tools, vacuum-supported suction to clean up the point of incision, and the transport of fluids. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
press photo Piezo technology for breathing Festo proportional regulators with piezo technology provide vital functions for uninterrupted breathing in anaesthesia devices. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
press photo Oxygen therapy Small, light, portable for maximum mobility, quiet for pleasant operation – all ensured by closed-loop-controlled valves which meter the oxygen supply as required, thus preventing unnecessary consumption. (Photo: Festo AG & Co. KG)
Seeing clearly, breathing freely
press photo VEMP Extremely precise control of pressures and gas flows: The proportional regulator VEMP with piezo technology is ideal for use in mobile devices. (Foto: Festo AG & Co. KG)
Handling viscose substances with precision
Festo press photo Bench-top platform Compact bench-top platform: The Modular Sample Processor is a system for preparing samples, such as for chromatographic analysis with high-pressure throughput. (Photo: Festo AG & Co. KG)
Handling viscose substances with precision
Festo press photo Pipetting procedures Precise pipetting procedures: Guaranteed by compact handling gantries with electric axes from Festo – the DGEA axis in the X-direction and the EGSK axis in the Y-direction, equipped with motors of the type EMMS-ST. (Photo: Festo AG & Co. KG)
Handling viscose substances with precision
Festo press photo Dispensing head Developing the dispensing head was no minor task either. After all, the samples have to be assigned to precisely the correct sample containers, with no room for errors. (Photo: Festo AG & Co. KG)
Handling viscose substances with precision
Festo press photo Markus Schöllauf "Thanks to the complete system solution, we were able to keep the short development time for our new sample processor," explains Markus Schoellauf from the Automation and Robotics division of Anton Paar. (Photo: Festo AG & Co. KG)
Mostrar 7 mais resultados ...