Портал технической поддержки

Выберите категорию из списка слева или воспользуйтесь поиском.

Поиск

Номер части

Серия

Код для заказа

Описание
CoDeSys version 3 - A hardware independent introduction to CoDeSys
CoDeSys version 3 - A hardware independent introduction to CoDeSys

Flexibility despite a high degree of automation is one of the most important challenges in manufacturing companies. It demands the integration and networking of different controls in a complex automation system. This is complicated by the huge variety of programming software available. Differences in user interface, functionality and command sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

Maintenance and troubleshooting of electropneumatic systems using PLC controls
Maintenance and troubleshooting of electropneumatic systems using PLC controls

This course allows you to extend your specialist knowledge of complex pneumatic systems and improve your methodological skills. Practical exercises on training equipment for setup, commissioning, troubleshooting and fault elimination facilitate the transfer of knowledge to your day-to-day work. 

Mastering the basics of electrical drives
Mastering the basics of electrical drives

As electrical drives are increasingly used in industry, many mechanical engineers and technicians are confronted with this new and initially complex technology and are expected to be able to commission and maintain it. This is a daunting prospect for anyone that has not had proper training. This course aims to provide this target group with the attitudes, skills and knowledge they need to master the basics. On completion of the training participants are able to select the most appropriate components for a given application, safely commission drives, and locate and eliminate simple faults.

Mastering machinery safety 2
Mastering machinery safety 2

When several machines are combined we are dealing with an Integrated Manufacturing System (IMS). Information about IMS can be found in the harmonised standard EN ISO 11161:2010 Safety of machinery – Integrated manufacturing systems – Basic requirements.

Mastering machinery safety 1
Mastering machinery safety 1

Since December 2009 it is compulsory to use the “new” machinery directive 2006/42/EC. This requirement together with the harmonised standards could translate into a significant change in your organization. Other than several small modifications and additions, the new IIB declaration (referred to as the declaration of incorporation) is also introduced. Technical files and user manuals with information about transportation, installation, commissioning, adjustment, maintenance, disassembly, scraping and recycling must be created and delivered with the partially completed machinery.

Systematic safety improvement in pneumatic systems
Systematic safety improvement in pneumatic systems

Just like good functionality and economic efficiency, safety is essential to the success of any product. What is more, the European directives and standards require intelligent solutions and raise the level of professional skills required. As a result, there is a wide range of different products, information and qualifications for safety engineering. However, most of them focus on the control level. This course familiarises participants with integrated control and pneumatic solutions for the right commissioning, troubleshooting, set-up, maintenance and simple optimisation of a system.

Energy saving in pneumatic systems
Energy saving in pneumatic systems

Saving energy is becoming more and more vital. In factories and even small workshops, the intelligent use of energy sources and rightsizing and selection of components can save time and substantially cut cost and waste. Compressed air is a key energy source for industrial production and offers huge potential for cost-saving – from production to consumption. Savings begin by paying attention to the people working with compressed air. This course focuses on peoples’ attention to costs and improvements the areas of compressed air production, preparation and distribution, as well as on the design of pneumatic circuits. This course particularly meets the training needs of customers who have already benefited from the Festo Energy Saving Service.

Vacuum in handling technology
Vacuum in handling technology

Vacuum plays an important role in handling technology. Vacuum is used in positioning, transporting, lifting, sorting and many other applications. Knowledge of vacuum technology is essential for those working with these applications, especially those who design and maintain them, or need to select appropriate vacuum components.

In this course, participants learn about the basic specifics of vacuum compared to compressed air. The main topics covered are production of vacuum, selection of the right suction cups, and opportunities for cost reduction.

CoDeSys version 2 - A hardware independent introduction to PLC programming
CoDeSys version 2 - A hardware independent introduction to PLC programming

In order to master the fast-changing requirements of embedded and PC-controlled industrial applications, it is increasingly important to master and apply different programming languages. This is complicated by the huge variety of programming software available. Differences in user-interface, functionality and commands sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

CoDeSys version 3 - A hardware independent introduction to PLC programming
CoDeSys version 3 - A hardware independent introduction to PLC programming

In order to master the fast-changing requirements of embedded and PC-controlled industrial applications, it is increasingly important to master and apply different programming languages. This is complicated by the huge variety of programming software available. Differences in user-interface, functionality and commands sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

Основы программирования в универсальной среде CoDeSys
Основы программирования в универсальной среде CoDeSys

Обзор стандарта IEC 61131-3.
Обзор контроллеров FESTO, программируемых с помощью CoDeSys.
Структура среды программирования CoDeSys.
Написание управляющих программ на языках LD, FBD, CFC.
Работа с различными эмуляторами контроллера.
Создание визуализации.
Применение функций, функциональных блоков и библиотек.
Подключение Target-пакетов.
Конфигурирование и параметрирование ПЛК с CoDeSys.
Контроль цикличности выполнения программ.
Отладка программ.
Экспорт и импорт программ CoDeSys.
Практические занятия по составлению, монтажу и наладке схем управления на стендах.
Использование интерактивной справочной системы

Основы функционирования систем промышленной пневмоавтоматики
Основы функционирования систем промышленной пневмоавтоматики

Структура пневматической системы
Условные обозначения и правила составления принципиальных пневмосхем по DIN ISO 1219
Устройства подготовки сжатого воздуха
Конструкция и принцип действия пневматических исполнительных механизмов
Применение и функционирование клапанов и пневматических распределителей (распределители с ручным, механическим и пневматическим управлением; клапаны давления, запорные клапаны, дроссели, реле и датчики)
Основные схемы управления
Практические упражнения. Разработка схем, сборка, отладка и проверка на учебных стендах, оснащенных промышленными комплектующими

Подписаться на RSS