Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
Motion Terminal Quick Reference PLC programming
Motion Terminal Quick Reference PLC programming VTEM

VTEM Motion Terminal Quick Reference PLC programming

1.10
2. 09. 2019
VTEM Firmware Download Instructions for V4.12.0
VTEM Firmware Download Instructions for V4.12.0 VTEM

This document provides a step-by-step explanation of how to download the newest VTEM Firmware using Festo Field Device Tool. This Application Note describes a one-time migration which is required for all firmware versions older than 4.12.0. If firmware is already 4.12.0 or higher the migration step with bootloader-5.1.0 and misc-1.0.0 is not necessary.

1.40
23. 07. 2019
Supported drives VTEM
Supported drives VTEM Festo Motion Terminal (VTEM)

This list contains all Festo drives approved for the Festo Motion Terminal (VTEM) and the corresponding value that must be entered in the

"drive type" system parameter (ID 20) in order to be able to operate the respective drive with a Motion App.

1.30
16. 05. 2019
Malfunction codes VTEM
Malfunction codes VTEM Festo Motion Terminal (VTEM)

The following tables contain all the malfunction codes and sub-codes relevant to the application that can be stored in the diagnostic memory of the Festo Motion Terminal (VTEM).

1.30
16. 05. 2019
Safety Sub-Functions in Connection with Motion Terminal VTEM
Safety Sub-Functions in Connection with Motion Terminal VTEM Motion Terminal VTEM

Safety Sub-Functions in Connection with Motion Terminal VTEM

1.33
23. 11. 2018
Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node
Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node VTEM; CPX-FB38

Commissioning VTEM connected to Beckoff PLC via CPX-FB38 bus node

1.10
24. 09. 2018
Servicevideos
Servicevideos service2see

(servicevideos)

Subscribe to RSS
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.