Control via Ethernet (CVE)
Title:
Control via Ethernet (CVE)
Subtitle:
CMMO-ST
Description:

This application note describes how to read the actual position and how to change the target position or velocity of position sets previously defined using FCT. It is an add-on to the descrip-tion "Control via Ethernet (CVE)" in the manual of the motor controller CMMO-ST-C5-1-DIO. Knowledge of CVE protocol as described in the manual is required.

Document type:
Application Note Control via Ethernet (CVE)
Title Version

This application note describes how to read the actual position and how to change the target position or velocity of position sets previously defined using FCT. It is an add-on to the descrip-tion "Control via Ethernet (CVE)" in the manual of the motor controller CMMO-ST-C5-1-DIO. Knowledge of CVE protocol as described in the manual is required.