Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description
Vacuum in handling technology
Vacuum in handling technology

Vacuum plays an important role in handling technology. Vacuum is used in positioning, transporting, lifting, sorting and many other applications. Knowledge of vacuum technology is essential for those working with these applications, especially those who design and maintain them, or need to select appropriate vacuum components.

In this course, participants learn about the basic specifics of vacuum compared to compressed air. The main topics covered are production of vacuum, selection of the right suction cups, and opportunities for cost reduction.

Energy saving in pneumatic systems
Energy saving in pneumatic systems

Saving energy is becoming more and more vital. In factories and even small workshops, the intelligent use of energy sources and rightsizing and selection of components can save time and substantially cut cost and waste. Compressed air is a key energy source for industrial production and offers huge potential for cost-saving – from production to consumption. Savings begin by paying attention to the people working with compressed air. This course focuses on peoples’ attention to costs and improvements the areas of compressed air production, preparation and distribution, as well as on the design of pneumatic circuits. This course particularly meets the training needs of customers who have already benefited from the Festo Energy Saving Service. 

Pneumatiska säkerhetsfunktioner
Pneumatiska säkerhetsfunktioner

Kursen vänder sig till alla som vill få fördjupade kunskaper om säkerhetsaspekterna vid uppbyggnad av pneumatiska system. Deltagaren får kunskap om komponentval och olika pneumatiska grundkopplingar utifrån ställda säkerhetskrav.

Vi går även igenom olika kontrollsekvenser, säkerhetssymboler enligt ISO 1219-1 och pneumatiska kopplingar enligt ISO 1219-2. Genomgång av den nya säkerhetsstandarden EN ISO 13849-1 och 13849-2 (denna nya standard ersätter tidigare EN 954-1). Kursen innehåller även avsnitt om riskbedömning.

Mastering machinery safety 1
Mastering machinery safety 1

Since December 2009 it is compulsory to use the “new” machinery directive 2006/42/EC. This requirement together with the harmonised standards could translate into a significant change in your organization. Other than several small modifications and additions, the new IIB declaration (referred to as the declaration of incorporation) is also introduced. Technical files and user manuals with information about transportation, installation, commissioning, adjustment, maintenance, disassembly, scraping and recycling must be created and delivered with the partially completed machinery.

Mastering machinery safety 2
Mastering machinery safety 2

When several machines are combined we are dealing with an Integrated Manufacturing System (IMS). Information about IMS can be found in the harmonised standard EN ISO 11161:2010 Safety of machinery – Integrated manufacturing systems – Basic requirements.

Explosive safety
Explosive safety

This course gives you an insight into standards-based explosive safety & explosion protection with risk analysis and operation/maintenance of electrical & mechanical installations. It also covers the development of explosive safety rules for machines, equipment and switchgear, conformity with the CE mark, explosive safety documentation as well as explosive safety in other countries.

Mastering the basics of electrical drives
Mastering the basics of electrical drives

As electrical drives are increasingly used in industry, many mechanical engineers and technicians are confronted with this new and initially complex technology and are expected to be able to commission and maintain it. This is a daunting prospect for anyone that has not had proper training. This course aims to provide this target group with the attitudes, skills and knowledge they need to master the basics. On completion of the training participants are able to select the most appropriate components for a given application, safely commission drives, and locate and eliminate simple faults.

Valve terminal CPX – Commissioning, modification and fault elimination
Valve terminal CPX – Commissioning, modification and fault elimination

Preconfigured complex systems with valve terminals and mechanical, pneumatic and electrical components bring numerous advantages but create new tasks for maintenance staff. This courses enables you to understand how pneumatic and electrical components work together. You will also learn identification and elimination of faults, and troubleshooting aids.

PLC-grundkurs med CoDeSys
PLC-grundkurs med CoDeSys

Deltagarna har efter genomgången kurs nödvändiga kunskaper för att arbeta effektivt med PLC-system med CoDeSys

CoDeSys version 3 - A hardware independent introduction to CoDeSys
CoDeSys version 3 - A hardware independent introduction to CoDeSys

Flexibility despite a high degree of automation is one of the most important challenges in manufacturing companies. It demands the integration and networking of different controls in a complex automation system. This is complicated by the huge variety of programming software available. Differences in user interface, functionality and command sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

Valves in Process Automation
Valves in Process Automation

This course provides you with insight into process valve technology, including valve/drive selection based on materials and standards, and taking cavitations into account. It also gives you an understanding of entire valve control systems.

Pneumatics for water management
Pneumatics for water management

There is a trend among operators of water treatment plants towards the increased use of pneumatic drives instead of electric drives. The advantages in terms of cost, system reliability, reduced complexity, ease of use and maintenance clearly speak for this technology.
This three-day course gives the participants an insight into process automation in water-related plants, making an important contribution to the process reliability of these plants.

Safe and efficient water transport and distribution
Safe and efficient water transport and distribution

Safe water transport and distribution is essential for drinking water supply. Participants of this module are familiarized with control technologies in water transport to achieve the optimum distribution of drinking water to the consumer. For this purpose all relevant components need to function efficiently and form an effectively adjusted system. The module traces the flow of water from the source to the public. Pumps are one of the focuses, since they are widely used in water plants.

Modern industriell pneumatik (pneumatik - grundkurs)
Modern industriell pneumatik (pneumatik - grundkurs)

Deltagarna har efter genomgången kurs nödvändiga kunskaper för att arbeta effektivt med pneumatik i produktionen

Maintenance and troubleshooting of electropneumatic systems using PLC controls
Maintenance and troubleshooting of electropneumatic systems using PLC controls

This course allows you to extend your specialist knowledge of complex pneumatic systems and improve your methodological skills. Practical exercises on training equipment for setup, commissioning, troubleshooting and fault elimination facilitate the transfer of knowledge to your day-to-day work. 

CoDeSys version 3 - A hardware independent introduction to PLC programming
CoDeSys version 3 - A hardware independent introduction to PLC programming

In order to master the fast-changing requirements of embedded and PC-controlled industrial applications, it is increasingly important to master and apply different programming languages. This is complicated by the huge variety of programming software available. Differences in user-interface, functionality and commands sets cause confusion and make mistakes more likely. CoDeSys – a tried and tested, globally-introduced hardware-independent software from 3S offers a Controller Development System according to the IEC 61131-3 with all defined programming languages independent of the hardware manufacturer. This training demystifies CoDeSys and gives participants confidence in using it.

Subscribe to RSS