2018/2/19

Moving loads at the tip of two fingers

Moving loads at the tip of two fingers

Intuitive balancer for improved ergonomics and safety
At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo.

Ergonomics improves efficiency thanks to a servo-pneumatic balancer that enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. At the heart of the balancer is the powerful and reliable drive solution YHBP from Festo with automatic weight detection and safety Performance Level d – perfect for the automotive and packaging industries.

 

The system automatically detects the weight of the load and sets the balancing force itself, even when suspended loads are added or removed. This makes production processes with a large number of variants much more flexible. And operation is child's play thanks to intuitive control using a pneumatically activated, ergonomic handle.

 

Playing it safe

Ergonomics must always go hand in hand with machine safety. The safety variant of the drive solution, with dual-channel speed monitoring and power shutdown, achieves Performance Level d. This ensures it is always brought to a safe state in the event of a faulty component. Dangerous movement is likewise prevented if there is a voltage failure or sudden drop in pressure.

 

The servo-pneumatic drive solution YHBP consists – depending on the version – of a pneumatic ISO cylinder with a diameter of 80 to 200 mm, a displacement encoder, optionally with safety relay for safety applications, the balancer valve unit VPCB, a pneumatically operative handle, the balancer controller CECC-D-BA for activation of the balancer. A balancer software with browser-based web visualisation is pre-installed on the controller for commissioning and diagnostics.

 

Kinematics and applications

The drive system has proven to be versatile and flexible, making it suitable for nearly all balancer kinematics, from lifting column to parallel kinematics and articulated-arm kinematics, regardless of whether it is standing or hanging, for example from a rail system.

 

In the automotive industry, the balancer can be used to move and precisely adjust heavy components, such as in the assembly of shock absorbers, engines, dashboards, tyres, windscreens, doors and seats. In the food processing and electronics industries, the balancer handles the loading and onward transportation of heavy containers, packages and goods. In the packaging industry, the focus is on conveying rolls of paper and film, and automated loading and repositioning of pallets. Similar applications can also be found in general machine and system building, in toolmaking, and in domestic appliances, heating and air conditioning engineering.

 

https://www.festo.com/cms/en-gb_gb/2462.htm

 

About Festo:

Festo AG is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 40 industries. The products and services are available in 176 countries. With about 18,800 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €2.74 billion in 2016. Each year around

8 % of this turnover is invested in research and development.

 

In this learning company, 1.5 % of turnover is invested in basic and further training. Yet training services are not only provided for Festo's own staff – Festo Didactic SE also supplies basic and further training programmes in the field of automation technology for customers, students and trainees.

问题:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo 媒体服务

 
 

图片

图片说明 下载
Festo press photo Balancer Ergonomics improves efficiency – thanks to a servo-pneumatic balancer with the drive solution YHBP from Festo. This enables employees in assembly and logistics to lift and move loads effortlessly, using just two fingers. (Photo: Festo AG & Co. KG)
Festo press photo balancer system and components Ingredients of the balancer servopneumatic system: pneumatic ISO cylinder, displacement encoder, optionally with safety relay, balancer valve unit VPCB, handle, balancer controller CECC-D-BA with balancer software with browser-based web visualisation. (Photo: Festo AG & Co. KG)