2018/5/16

Fast and reliable configuration of automated process valves

Fast and reliable configuration of automated process valves

The new configurator from Festo saves time and money
The configurator for process valve units significantly simplifies engineering and procurement processes.

 

From manually operated to automated process   valves, the new configurator for process valves from Festo makes selecting   the optimum solution child's play. Simply select a few parameters and the   configurator will immediately suggest appropriate combinations, making   engineering in the process industry fast, reliable and easy.

 

The configurator for process valve units significantly simplifies engineering and procurement processes. The tool ensures quick and successful project management by taking all relevant factors into account: from initial product search, configuration, sizing and documentation right through to ordering and delivery of the ready-to-install process valve unit – including customer-specific requests, everything is combined in one tool.

 

Configurated process valve units are tailored and ready-to-install, all components are perfectly matched: butterfly valves, quarter turn actuators, pilot valves, sensor boxes, positioners, adapter kits and hand levers. Whatever you are looking for, whether it is the ease of manually actuated combinations, a unit with pilot valves and a sensor box, or a unit with a positioner, you simply choose the required parameters in the input menu and the configurator suggests the right solutions.

 

Order ID and CAD download included

Together with the proposed solution, the configurator generates an order ID for the complete combination, which can be used for placing future orders. There are also benefits in terms of documentation because the CAD data for the complete module can be downloaded in accordance with the configuration.

 

Breakthrough in digitalisation

With its configurator for process valve units, Festo is driving digitalisation and supporting its customers to enter the age of Industry 4.0. Festo as an automation expert is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation practice.

 

Festo is also using digital communication to support its customers throughout the Digital Customer Journey. This digital journey guides users safely and comprehensively through the Festo portfolio, from information procurement and configuration through ordering and delivery to commissioning and maintenance or even to the technical training offering of Festo Didactic.

 

Link to the configurator:

www.festo.com/kvza

问题:

Christopher Haug

+49(711)347-4032
+49 (0) 711-34754-4032

Festo 媒体服务

 
 

图片

图片说明 下载
Configurator for process valve units 1 Get the right solution quickly and easily with the configurator for process valve units. (Photo: Festo AG & Co. KG)
Configurator for process valve units 2 Get the right solution quickly and easily with the configurator for process valve units. (Photo: Festo AG & Co. KG)