2018/11/30

The right handling system in a matter of minutes

The right handling system in a matter of minutes

Handling Guide Online with many Cartesian robots and commissioning files
The Handling Guide Online enables engineers to design the right ready-to-install handling system from Festo in record time

The   Handling Guide Online enables engineers to design the right ready-to-install   handling system from Festo in record time, whether it is a single-axis   system, a two-dimensional linear and planar surface gantry or a   three-dimensional gantry. From 2019, the configuration and ordering software   will comprise particularly compact, but also highly dynamic Cartesian robots from Festo.

 

This includes Cartesian high-speed robots based on EXCT with 90 picks a minute, as well as planar surface gantries based on the EXCH series, which achieve cycle rates of 100 picks a minute. The particularly compact planar surface gantries and 3-dimensional gantries of the EXCM series are ideal for desktop applications in small parts assembly, electronics manufacturing or laboratory processes.

 

Complete value chain

In Festo’s Handling Guide Online design and project engineers have a smart and intuitive tool to configure and create new system solutions; and since the new configuration and ordering platform is integrated into Festo’s online product catalogue there is no need to interrupt the value chain. They can have the right standard handling system, including CAD model, in just a few mouse clicks. The individual steps including RFQ, layout, quotation and CAD design, which previously took 10 to 15 days, can now be done in just a matter of minutes using the Handling Guide Online.

 

The Handling Guide Online opens up entirely new horizons with standardised handling systems. It revolutionises assembly and delivery times, reducing them from nearly two months to just a few weeks. New standard products are also shortening parameterisation and commissioning times. Machine and equipment manufacturers are thus able to reduce their time-to-market for integrated handling systems by around 70%. Thanks to this engineering tool, design engineers have more time and space for creativity in planning and project engineering processes for their companies’ core areas of technological expertise.

 

Just a few steps to a handling system

Just a few steps are all it takes to arrive at a fully configured handling system. In the first step, the design engineer selects the required type of handling system and enters the application data in the Handling Guide Online. The tool calculates and suggests appropriate handling systems.

 

The planner then selects the most suitable handling system from these suggestions. The data sheet and the correctly configured CAD model are immediately available for download in all common data formats for direct integration into the customer’s own design engineering system. The engineer then uses additional options to configure the selected system in accordance with their own requirements.

 

The selected handling system is then transferred to the shopping basket. A final click transmits the order to Festo. Festo’s handling experts deliver a ready-to-install system, including all user documentation in accordance with the EU Machinery Directive, directly to the machine or plant in no time at all.

 

Efficient commissioning

Festo now offers commissioning files for fast commissioning. The files are custom created on the basis of user input and the calculated system and can be loaded directly into the motor controller. The commissioning file contains a set of values specifically for the handling system, consisting of axis dimensions, motor characteristics, feed constants and dynamic data.

 

A special feature is that the controller settings are automatically calculated on the basis of the payload, the dead weight and the system dynamics entered by the user. This enables users to shorten their time-to-market.

 

Breakthrough in digitalisation

With the Handling Guide Online, Festo is driving digitalisation forward and supporting its customers to enter the age of Industry 4.0. Automation expert Festo is combining its extensive knowledge of industrial applications with the latest developments in information technology to realise online applications for industrial automation practice. Festo is also using digital communication to support its customers throughout the Digital Customer Journey. This digital journey guides customers reliably and comprehensively through the Festo portfolio, from information procurement and configuration through ordering and delivery to commissioning and maintenance or even to the technical training offering of Festo Didactic.

 

 

Please   refer to:

Festo   press image of the Handling Guide Online monitor

 

                                                                          

Caption:

With the Handling Guide Online, machine   and equipment manufacturers are able to reduce their time-to-market for   integrated handling systems by up to 70%.

(photo: Festo AG & Co. KG)

 

 

About Festo:

Festo AG is a global player and an independent family-owned company with headquarters in Esslingen am Neckar, Germany. The company supplies pneumatic and electrical automation technology to 300,000 customers of factory and process automation in over 35 industries. The products and services are available in 176 countries. With about 20,100 employees in over 250 branch offices in 61 countries worldwide, Festo achieved a turnover of around €3.1 billion in 2017. Each year around    8 % of this turnover is invested in research and development.

 

In this learning company, 1.5 % of turnover is invested in basic and further training. Yet training services are not only provided for Festo's own staff – Festo Didactic SE also supplies basic and further training programmes in the field of automation technology for customers, students and trainees.

 

Further information:

Press text and photos are also available online at www.festo.com/press.

Or mobile at http://m.festo.com/press.

 

For queries please contact:

Festo AG & Co. KG

Christopher Haug, Customer Magazine and Technical Press

phone: +49 711-347 4032, E-Mail: christopher.haug@festo.com

 

Festo in Social Media:

Facebook:    www.festo.com/facebook

Twitter:         www.festo.com/twitter

LinkedIn:      www.festo.com/linkedin

Youtube:      www.festo.com/youtube

问题:

Christopher Haug

+49(711)347-4032
+49(711)34754-4032

Festo 媒体服务

 
 

图片

图片说明 下载
Festo press image of the Handling Guide Online monitor With the Handling Guide Online, machine and equipment manufacturers are able to reduce their time-to-market for integrated handling systems by up to 70%. (photo: Festo AG & Co. KG)