Festo 媒体服务

请在左侧目录中选择或使用搜索功能。

图片说明 下载
Ready-to-install solutions for the lab-on-a-chip
Festo Press Image Festo LifeTech Mobile analytical devices allow fast testing to identify pathogens in the case of colds or flu-like infections as well as other bacterial or viral diseases. (Photo: Festo AG & Co. KG)
Ready-to-install solutions for the lab-on-a-chip
Festo Press Image Valve assembly in vitro diagnostics In vitro diagnostics made easy with a ready-to-install valve block for controlling the cartridges in bench-top units. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image Head Office The corporate head office of Festo at Esslingen a.N., Germany. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image laboratory automation Festo develops intelligent, tested subsystems for the automation of liquid media and sample handling applications. The applications involve the use of both electric and pneumatic actuators with motors, controllers and handling systems, as well as grippers, sensors and camera systems. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image medical technology In medical technology, the focus is on the efficient open-loop and closed-loop control of medical gases. (Photo: Festo AG & Co. KG)
Precisely dispensed
Planar surface gantry for laboratory automation The best possible solution for system manufacturers: as well as its own components such as the planar surface gantry EXCM, Festo also integrates components from third-party manufacturers. (Photo: Festo AG & Co. KG)
Precisely dispensed
Pipetting into microplates The various process steps for adding different liquids to microplates are automated and linked in a very compact space. (Photo: Festo AG & Co. KG)
Precisely dispensed
VTOE Contactless dispensing of very small volumes: the 8-channel dispense head VTOE is a configurable complete solution comprising manifold duct plate, dosing valves and nozzles. (Photo: Festo AG & Co. KG)
Precisely dispensed
VYKA The media separated solenoid valve VYKA allows the precise dispensing of fluids and the control of liquid flows in manifold duct plates. (Photo: Festo AG & Co. KG)
Precisely dispensed
VAEM The VAEM valve control module with holding current reduction is ideal for controlling dosing heads. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 1 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Adaptive Shape Gripper 2 The adaptive shape gripper DHEF grips formless, round and sensitive objects – as the tongue of a chameleon does. (Photo: Festo AG & Co. KG)
The automated chameleon tongue
Stefanie Seiler and Nenja Rieskamp These two Festo colleagues developed the adaptive form gripper DHEF from a bionic prototype to a catalogue product: Stefanie Seiler (Product Management, on the left) und Nenja Rieskamp (Product Development) (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image Head Office The corporate head office of Festo at Esslingen a.N., Germany. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image laboratory automation Festo develops intelligent, tested subsystems for the automation of liquid media and sample handling applications. The applications involve the use of both electric and pneumatic actuators with motors, controllers and handling systems, as well as grippers, sensors and camera systems. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image medical technology In medical technology, the focus is on the efficient open-loop and closed-loop control of medical gases. Proportional valves with piezo technology are often used in both mobile applications and applications involving the treatment of patients at their bedsides. (Photo: Festo AG & Co. KG)
The Festo Group
Festo Press Image CP Factory Qualification for Industry 4.0: Festo Didactic offers a cyber-physical learning and research platform in the form of the CP Factory. This platform models the stations in a real production plant. (Photo: Festo Didactic SE)
Extremely precise incisions
QUBE pro 1 Technical assistant of choice for eye surgeons: the QUBE pro takes individual working methods into consideration and has a dual linear control pedal. (Photo: Festo AG & Co. KG)
Extremely precise incisions
QUBE pro 2 Highly precise incisions: thanks to fast-switching valves from Festo, the QUBE pro achieves rates of up to 7500 cuts per minute in order to be able to use the cutter accurately. (Photo: Festo AG & Co. KG)
Extremely precise incisions
Valve control block in the QUBE pro 50% less installation space than a conventional solution with numerous individual tubing connections for each pneumatic component: the valve control block in the QUBE pro. (Photo: Festo AG & Co. KG)
Extremely precise incisions
Valve control block It hardly gets any more compact than this: control block with proportional, piezo and fast-switching valves and manifold duct plates with integration technology. (Photo: Festo AG & Co. KG)
Extremely precise incisions
Paul Willi Coenen "The fast-switching valves from Festo made it possible for the very first time to achieve the required cutting speed for the QUBE pro,” says Paul Willi Coenen, President and CEO of BYTEC. (Photo: Festo AG & Co. KG)
Measuring, weighing and transporting without contact
Festo Press Image SupraSensor_1 The SupraSensor exhibit consists of a hermetically sealed liquid-filled tube positioned over a high-precision balance, to which a cryostat with a superconductor is fixed. (Photo: Festo AG & Co. KG)
Measuring, weighing and transporting without contact
Festo Press Image SupraSensor_2 The concept SupraSensor allows various physical quantities, such as weight, density, viscosity or temperature, to be measured using a force-based measuring system. (Photo: Festo AG & Co. KG)
Measuring, weighing and transporting without contact
Festo Press Images SupraTransport_1, SupraTransport_2 An L-shaped workpiece carrier hovers above a magnetic rail with a large gap thanks to a permanent magnet on its underside – stabilised by superconductor technology. (Photos: Festo AG & Co. KG)
Measuring, weighing and transporting without contact
Festo Press Images SupraTransport_1, SupraTransport_2 An L-shaped workpiece carrier hovers above a magnetic rail with a large gap thanks to a permanent magnet on its underside – stabilised by superconductor technology. (Photos: Festo AG & Co. KG)
Festo opens development center in Boston
Festo Press Image TEC Boston On October 10, 2018, the automation specialist Festo will ceremoniously open its first development center for components and automation solutions specifically for the life science market in Boston. Photo: CBRE/New England)
Festo opens development center in Boston
Festo Press Image laboratory automation Festo develops intelligent, tested subsystems for the automation of liquid and sample handling. Photo: Festo AG & Co. KG)
Festo opens development center in Boston
Festo Press Image EHMD The compact EHMD rotary gripper module is unique on the market to date and can both grip and open sample vials. (Photo: Festo AG & Co. KG)
Festo opens development center in Boston
Festo Press Image VTOE-8 Precise dosing of various filling volumes and liquids with high throughput: the 8-channel dispense head VTOE-8. (Photo: Festo AG & Co. KG)
Festo opens development center in Boston
Festo Press Image medical technology In medical technology, the focus is on the efficient regulation and control of gases for medical devices. (Photo: Festo AG & Co. KG)
显示 30 更多结果……