﻿WEBVTT

00:12.697 --> 00:16.247
The company STAMA was looking for
a competent automation supplier

00:16.251 --> 00:18.476
for our new
milling-turning centres.

00:18.501 --> 00:20.079
The requirements here were:

00:20.149 --> 00:24.338
A space-saving design for accommodating
the machinery in the working space,

00:27.518 --> 00:32.318
all automation components to be well
sealed against chips and emulsion,

00:33.523 --> 00:35.978
a flexible length layout
of the automation beam

00:36.003 --> 00:37.879
for different pick-up positions

00:38.203 --> 00:40.408
as well as being optionally
equipped with a single

00:40.433 --> 00:43.477
or double gripper for
corresponding applications.

00:44.775 --> 00:46.970
Festo fulfilled all
this perfectly.

00:47.187 --> 00:49.683
That is why we opted for
Festo in this case.

00:49.864 --> 00:51.855
Last but not least, of
course, there were also

00:51.880 --> 00:55.868
criteria such as the good working
relationship with Festo over many years

00:55.904 --> 00:59.637
and the short distance of approx.
30 minutes from Festo headquarters

00:59.662 --> 01:03.061
to Stama headquarters
in Schlierbach.

01:23.689 --> 01:26.922
Our milling-turning centres, besides
having many other advantages,

01:26.966 --> 01:29.166
can also be retooled
very easily.

01:29.663 --> 01:32.411
This also relates to the
tool management, of course.

01:32.777 --> 01:35.919
That was implemented very well
here by working with Festo –

01:36.277 --> 01:38.591
and actually in the form
of a handling solution to

01:38.616 --> 01:41.274
bring the tools from the
inactive tooling magazine

01:41.302 --> 01:44.694
behind the machine to the
machine’s active magazine

01:45.048 --> 01:49.278
and hence to prepare the machine with
the right tools for the next order.

01:50.265 --> 01:53.067
Here too we worked with
Festo to create a very good

01:53.092 --> 01:56.758
solution which is very well
received by our customers.