除關鍵的增值型加工與組裝流程外,整合式機器人夾爪乃至真空吸盤等 EOAT 解決方案,同樣能顯著提升 OEE 並優化生產流程。 本文將為您闡釋 EOAT 如何協助實現高 OEE,並介紹其在可用性、性能與品質三大層面上的關鍵作用。
In industrial production, OEE is a key metric for visualising the productivity of an entire system. It is made up of three factors:
1. Availability: The time needed for the systems to be ready for use.
2. Performance: The speed of production.
3. Quality: The proportion of flawless products.
End effectors that handle sheet metal parts in production have an impact on all three factors. They offer project planners and designers numerous starting points, from quick changeovers to safe handling, for increasing production efficiency.
Frequent product changes and a wide range of models are the norm in the automotive industry. A flexible EOAT solution such as an adjustable pneumatic or mechanical robot gripper enables quick and easy changeovers. Instead of time-consuming installations, the gripping range of a vacuum lifter, for example, can be automatically adjusted using integrated adjustment components.
The result: minimised set-up times optimise system availability and increase productivity in the long term.
Unplanned failures are a productivity killer. Components for modern EOAT solutions are sturdy and durable, thus contributing to trouble-free operation. In addition, by monitoring status data such as pressure, vacuum level or component presence in real time, potentially dangerous situations can be identified at an early stage and prevented. Digital monitoring systems not only enable increased availability, but also ensure greater transparency and predictability in production processes.
EOAT systems with components from Festo are not only powerful, but also energy-efficient. Vacuum lifters with optimised air consumption reduce energy requirements without compromising on performance. This not only reduces production costs, but also contributes to the energy efficiency of the production processes, thusminimising resource consumption per workpiece. This approach turns the increase in production efficiency into a measurable competitive advantage.
Another important aspect of automated production is flexibility. Integrated robot grippers, which can handle different gripping points or clamping points, enable different workpiece sizes or geometries to be continuously transported without any loss of performance. It is thanks to this versatility that a flexible EOAT solution becomes a performance-enhancing tool in versatile automotive production.
Example: In the automated assembly of car body parts, adjustable gripper configurations can be programmed for different component geometries, eliminating changeover times. Parts with different formats can be picked up and passed on immediately. These automatically adjustable end effectors improve flexibility, support smooth production and ensure maximum production planning.
In addition to the classic OEE factors, the topic of sustainability is becoming increasingly important in the automotive industry. Modern EOAT solutions such as energy-optimised vacuum lifters reduce the consumption of resources and contribute to more environmentally friendly production. This not only meets legal requirements but is also in line with expectations of customers and investors, who are increasingly placing more value on sustainable processes.
Combining digital technologies with EOAT solutions offers new opportunities for optimisingproduction processes. IoT-enabled robot grippers can be used to efficiently carry out condition monitoring and predictive maintenance. With real-time data, the maintenance measures of production lines can be proactively controlled, resulting inminimised downtime.
A practical example: an integrated end effector with electric axes, which uses digital support to detect irregularities in the axis movement and alerts the maintenance team at an early stage, prevents unplanned production stops and ensures maximum availability.