The core challenge of process reliability and what is overlooked by many

Hydrogen is highly reactive and is often handled under enormous pressure, whether during the electrolysis of water, compression in high-pressure tanks or distribution in mobile trailers or filling stations. The molecule is also very small, which makes it more susceptible to leakage. Reliability is the top priority for all applications in the hydrogen value chain. Because in an emergency, people, systems and budgets can be jeopardised. This means that processes are sensitive at every stage of the value chain. It is important to keep these aspects in mind:

If you cut corners here or consider requirements too late, you not only run the risk of facing delays but also expensive retrofits. Find out in our blog post on functional safety using the example of hydrogen production how you can minimise risks right from the start by using a reliable safety concept.

10 Common Mistakes to Avoid in Hydrogen Automation ​

Hydrogen automation is complex, and mistakes can be costly. This checklist helps you prevent risks and design safer, scalable systems. You’ll learn how to: ​

  • Avoid the 10 most common errors ​
  • Save time and reduce rework ​
  • Strengthen safety and compliance
Get your free Checklist today

What if the tried and tested approach is not the best decision?

Traditional installations in the chemical and process industry often rely on individual valves mounted directly on the actuator. With numerous valves, sensors and controllers, the density of interfaces is high. Modern hydrogen systems often rely on modular units. While this facilitates integration into the overall system, this approach also increases the complexity of the individual modules. Without a consistent system architecture, this often leads to:

  • Compatibility problems that delay commissioning
  • Higher costs due to more time-consuming troubleshooting and
  • More maintenance work than necessary

This can be prevented with a sophisticated architecture and the right products. This is where compact valve terminals are a real game changer: their installation and maintenance costs are lower, they have centralised diagnostic options and are extremely modular for adaptations and expansions at a later stage.

Example: compact, modular valve terminal solutions such as VTUG or CPX-MPA combine controller, valves and monitoring in a single system. Depending on the application, they fulfil SIL requirements, are particularly suitable for harsh environments and can be used not only in stationary but also in mobile applications.

Why a lack of foresight can turn out to be expensive

The hydrogen market is growing rapidly. A glance at the EU hydrogen strategy alone (target: an electrolysis capacity of 40 GW by 2030) shows that the technical infrastructure must therefore be scalable. Without a coherent automation architecture there is risk of:

  • High conversion costs for capacity expansions
  • Project delays caused by renewed certifications
  • Limited flexibility in the event of market changes
  • Safety risks caused by inconsistent system integration

Choosing a sophisticated and coherent architecture at an early stage is the best way to avoid these problems. We can help you. We will make sure that your system is safe, efficient and scalable right from the start, whether it's with a ready-to-install control cabinet system, certified valve technology, modular pneumatics or engineering support in every phase of the project.

There is no energy transition without sophisticated automation

The challenges in the automation of hydrogen processes are real but can be solved. Choosing the right partners and concepts from the outset reduces risks, accelerates projects and creates the basis for long-term success.

What needs to be taken into account:

  • A comprehensive view of your application, from safety to integration to servicing.
  • A well-thought-out automation concept that enables scalability and conforms to standards.
  • Technologies and components that are suitable for the special requirements of hydrogen.
  • An automation solution that is cost-effective despite high production costs.