TL;DR

When using a CPX-AP-x-4IOL-M12 module on an EtherNet/IP network, it is recommended to use the non-OE Variant for selecting the port size. This way, you won’t have to deal with OutputEnable.

Description of OE

When configuring the ports of an IO-Link master like CPX-AP-I-4IOL-M12 or CPX-AP-A-4IOL-M12, you will come across a parameter that specifies the number of bytes reserved per IO-Link port, known as the Variant.

Let’s discuss setting up an IO-Link module for 2 bytes per port in an EtherNet/IP (EP) network. As shown in Figure 1, we have two options: Variant 2 and Variant 2_OE, both of which are supported on EP. The main difference lies in the output size, with Variant 2_OE having an additional 4 bytes.

Disclaimer

This post is provided solely for the purpose of offering setup assistance and general guidance. It is important to note that the ultimate responsibility for ensuring the overall safety and proper functionality of the machine lies with the System Integrator / End User. It is crucial to exercise caution, adhere to proper safety protocols, and consult relevant experts or professionals when necessary.

Although Festo employees will be contributing to this blog, please note this is not the official Festo support channel. For more timely technical support please reach out to your regional Festo support channel and/or consult user manuals and relevant documentation.