To utilize the CDPX-X-E1-W-‘X’ as a Codesys PLC, a Target Support Package is required. It is advisable to use a package that aligns with your Codesys version to ensure compatibility, although this is not strictly mandatory.
Example:
The latest CDPX Target Support Package is included in the Designer Studio packages starting from version 4.5.0.224. After installation of Designer Studio V4.5, you can locate the supporting CDPX Codesys Target Support Package in the following directory:
C:\Program Files (x86)\Festo\Designer Studio 4.5\CODESYS\V3
This post is provided solely for the purpose of offering setup assistance and general guidance. It is important to note that the ultimate responsibility for ensuring the overall safety and proper functionality of the machine lies with the System Integrator / End User. It is crucial to exercise caution, adhere to proper safety protocols, and consult relevant experts or professionals when necessary.
Although Festo employees will be contributing to this blog, please note this is not the official Festo support channel. For more timely technical support please reach out to your regional Festo support channel and/or consult user manuals and relevant documentation.