1. Energy efficiency: A key to reducing costs

Energy costs are a significant factor in the manufacture of semiconductors. In semiconductor production, the quality, reliability and performance of the semiconductor components produced depend on high-purity nitrogen. Its production with an air separation plant in the company is very energy-intensive.

The lithography process, in which tiny structures are transferred to the surface of the wafer using energy-intensive exposure devices, also requires a great deal of energy. As the production of semiconductors is almost completely automated, there is great potential for saving energy in the field of automation technology. With regular monitoring, you can identify inefficient processes and uncover potential savings in your company.

2. Materials management: Resource efficiency as a success factor in your company

The efficient use of raw materials and consumables plays a decisive role in cost optimization in semiconductor production. Companies can reduce their storage costs through precise inventory management and the avoidance of excess stock. Targeted and efficient use of materials reduces your operating costs and increases your economic and ecological success.

With the optimized and precise application of expensive photoresists, for example, you can achieve high-quality results and minimize waste. There is further potential for savings in the use of process gases, which are used for etching and coating. Special stainless steel valves are used for reliable and safe control of the gas flow.

Efficient use and system configuration through advanced process control and monitoring systems optimize the consumption of process gases in semiconductor manufacturing. This allows you to achieve considerable cost savings in your company.

3. Maintenance strategy: Prevention instead of reaction

Carefully planned and regular maintenance minimizes unplanned downtimes in the production of semiconductors and the associated loss of wafers in the process.

By using AI systems in semiconductor production, you can use the algorithms to analyze large volumes of production data and identify patterns that indicate anomalies or deviations. This allows you to identify potential problems at an early stage and react quickly through predictive maintenance. This predictive troubleshooting keeps product quality and efficiency at a high level, avoids rejects and helps to maximize the yield of the entire production.

4. Environmental management: Combining sustainability and cost savings

Effective waste management in semiconductor production is important from both an ecological and an economic point of view. By handling waste and chemicals correctly, you can achieve not only sustainable goals, but also considerable cost savings. For efficient and effective filtering of exhaust gases, special valves enable precise control and management of the gas flow.

Certain chemicals and substances used in semiconductor manufacturing can also get into the wastewater. With specific agents and the use of filters, these substances can be effectively removed from the wastewater and separated in an environmentally friendly manner.

Conclusion: increasing efficiency and sustainability in semiconductor manufacturing

Understanding the factors influencing operating costs is crucial for semiconductor manufacturers, so they can reduce them, which leads to sustainability and success in the long term. Even small factors can have a big influence.

Explore automation solutions for the semiconductor industry to see how Festo supports stable, efficient semiconductor production.

You can significantly reduce your company's operating costs and maximize profitability and competitiveness through optimized plant maintenance, improved and energy-efficient processes, effective environmental management and strategic material management in procurement, storage and production. Taking a comprehensive view of all aspects that can optimize costs and increase output throughout production is the key to success in the semiconductor industry.