What is green hydrogen?

Hydrogen is produced by electrolysis – a process in which water is split into hydrogen and oxygen using electricity. The following applies to green hydrogen production: the electricity used must come from renewable sources.

In contrast, for example:

  • Gray hydrogen produced from fossil fuels
  • Pink hydrogen, which does not emit CO₂ because nuclear energy is used, although radioactive waste is generated
  • Blue hydrogen, in which CO₂ is captured and stored (carbon capture).

Electrolysis is therefore the first – and decisive – step in the hydrogen value chain.

Discover how automation can improve processes along the entire value chain.

1. Production

The starting point in the hydrogen value chain is electrolysis. Water is broken down into hydrogen and oxygen using electricity from renewable energy sources. Different electrolyzer technologies are used depending on the framework conditions:

  • PEM for flexible load changes
  • Alkaline processes, based on proven processes
  • SOEC for maximum efficiency through high-temperature electrolysis

An automated control system ensures that the temperature, pressure and media flow are always within the optimum range – for maximum efficiency and system availability.

2. Hydrogen treatment

Freshly produced hydrogen is rarely immediately pure. It often contains moisture, oxygen residues, or other impurities. Special systems for hydrogen treatment bring it to the required quality – up to 99.999% pure. This is a decisive factor in preventing corrosion, loss of efficiency, or damage to downstream systems. Automated systems monitor all relevant process parameters in real time, react to deviations, and optimize the use of energy and operating resources. This not only increases security, but also makes the entire process more efficient and easier to scale.

3. Compression and storage

Hydrogen has a very low energy density at normal pressure. There are several ways to transport or store it efficiently:

  • as a compressed gasusing compressors from 350 up to 500 bar,
  • liquefaction by powerful cooling, or
  • chemical conversion of the molecule into hydrogen-containing compounds.

Pressure control, filling, and monitoring must be seamless and reliable. Precise valve technology and reliable sensors ensure stable, safe operation.

4. Distribution and transportation

The route from the production site to the place of use can look very different: from pipelines or trailers through to on-site production, anything is possible. In any event, transportation must be safe, economical, and involve low losses. Automated monitoring systems detect leaks or pressure fluctuations at an early stage, and control the flow rate and valve positions in real time.

5. Application

Green hydrogen has a wide range of applications. It can be used directly as a molecule in the chemical industry and for steel production, and is employed in the production of synthetic natural gas or fuels. Hydrogen can then be used again in fuel cells to generate electricity and thus contribute to a reduction in CO2 emissions from mobility in corresponding vehicles. Every application brings its own challenges – automation technology helps to master these reliably and flexibly. Processes can thus be adapted to changing conditions and load profiles at any time and fulfill important safety requirements.

10 Common Mistakes to Avoid in Hydrogen Automation

Hydrogen automation is complex, and mistakes can be costly. This checklist helps you prevent risks and design safer, scalable systems. You’ll learn how to:​

  • Avoid the 10 most common errors​
  • Save time and reduce rework​
  • Strengthen safety and compliance
Get your free Checklist today

Why automation is a key to scaling

Green hydrogen is only competitive if it can be produced and used safely, reliably, and efficiently. Automation solutions with valve manifolds and modular control units in combination with real-time diagnostic functions make this possible. Among other things, they help to:

  • Minimize downtimes
  • Fulfill regulatory requirements (ATEX, SIL)
  • Reduce complexity in the systems

Festo – your partner along the entire value chain

Festo supports companies along the entire hydrogen value chain with industry-specific automation solutions. Whether in electrolysis, gas treatment, or mobile applications such as trailer control systems – with scalable systems, digital diagnostic functions, and certified components, Festo helps to make processes safe and provides scope for future developments.

The green hydrogen value chain is more than just a topic for the future

It is already a reality today, and its importance is growing all the time. Those who understand the entire chain can make well-founded decisions and integrate suitable solutions at an early stage.

Are you getting curious?

Control hydrogen efficiently with Festo – from start to finish

Are you already working on a specific application?

Talk to our experts about your automation solution