Hardware and Software used

Hardware:

  • Servo drive CMMT-ST-C8-1C-MP-S0

Software Versions:

  • Festo Automation Suite V2.8.0.417
  • CMMT-ST Plug-in V2.8.2.0
  • Scan extension V2.8.1.40

Backup with Festo Automation Suite

Festo’s CMMT servo drives family offers several ways to obtain a backup of the contained configuration, but for this note we will focus on the option through the Festo Automation Suite.

But why is it important to obtain a backup? The answer is simple, this configuration describes the hardware that is controlled by the servo drive, as well as the application parameters such as working load, stroke, among other important parameters. It is a good practice to obtain the configuration backups when the equipment is installed for production purposes.

To start the process, you must open Festo Automation Suite and choose the “New Project” option. The software will display an environment like this one:

Disclaimer

This post is provided solely for the purpose of offering setup assistance and general guidance. It is important to note that the ultimate responsibility for ensuring the overall safety and proper functionality of the machine lies with the System Integrator / End User. It is crucial to exercise caution, adhere to proper safety protocols, and consult relevant experts or professionals when necessary.

Although Festo employees will be contributing to this blog, please note this is not the official Festo support channel. For more timely technical support please reach out to your regional Festo support channel and/or consult user manuals and relevant documentation.