Typical contaminants in one cubic meter of unprepared ambient air can include:
When this air is compressed, all these contaminants become more concentrated. Without proper preparation, they can enter the compressed air network and negatively affect components, processes, and product quality.
These particles can cause:
Over time, particle contamination reduces system reliability and shortens the service life of pneumatic components.
Ambient air always contains water vapor. During compression and subsequent cooling, this vapor condenses into liquid water. If it is not removed effectively, this water can spread throughout the compressed air system.
The consequences include:
Water is one of the most common and critical contaminants in compressed air systems and must be managed systematically.
Even in systems with oil-free compressors, oil contamination can still occur. Sources include:
Oil in the compressed air can lead to:
In many industries, even very small amounts of oil can be unacceptable and must be removed reliably.
If compressed air contamination is not addressed, the effects are often seen across the entire lifecycle of the system:
Systematic air preparation and maintenance are therefore not only technical necessities, but also key levers for cost and quality optimization.
Different industries place different demands on compressed air quality:
Many sectors refer to standards such as ISO 8573-1, which define compressed air purity classes for particles, water, and oil. Customer specifications and local regulations typically specify the required purity class. The target air quality should always be defined based on the specific application and aligned with the latest standards, customer requirements, and applicable regulations.
Effective compressed air preparation combines suitable equipment with consistent maintenance. Both are essential for achieving and maintaining the required air quality over the entire service life of the system. Modern air preparation systems integrate several functions to address the main sources of contamination:
Even the best air preparation equipment can only perform reliably if it is maintained regularly. Structured maintenance supports stable operation, compliance with standards, and energy-efficient system performance.
Key maintenance tasks include:
Filters gradually become loaded with contaminants. Timely replacement ensures consistent filtration performance, prevents blockages, and avoids excessive differential pressure that would increase energy consumption.
Regular monitoring of the pressure dew point helps verify that dryers are working correctly and that the required moisture levels are maintained.This is particularly important in applications with strict dew point requirements or in environments where low temperatures can cause freezing.
A documented maintenance strategy, aligned with manufacturer recommendations and application requirements, is a key element of sustainable compressed air management.