搬運系統和工業機器人

藉由搬運系統和工業機器人,可以盡可能實現工件搬運自動化,例如抓取、定位、堆放、分組或分度。因此,搬運系統能夠確保順利、高效地在完全自動化過程中完成物料運輸。透過投資搬運系統,製造公司可以節約成本,顯著提高生產力。自動化技術同機器人技術和搬運密切相關,這涵蓋了搬運工件所需的編程和控制過程。Festo 是全球自動化領域的領導企業:從專案規劃到生產,再到整合,我們會用我們的專業訣竅伴隨客戶實施整個過程。

Festo 搬運系統和機器人

我們為組裝和搬運領域的各種應用提供搬運系統:從自動化技術領域常見應用的標準解決方案,到滿足您具體要求的個人化解決方案,應有盡有。在生產中,除了整個設備的數位互聯,自學系統和基於機器人的自動化解決方案也日益發揮決定性的作用。因此,我們的產品範圍包括氣動搬運系統和相對應的控制系統,以及笛卡爾機器人並聯三角式機器人

Parallel kinematic system robots

Our delta robots with parallel kinematics are also ready-to-install systems. They are used for freely positioning parts in three-dimensional workspaces. The industrial robots provide excellent precision in movement and positioning as well as exceptionally high dynamic response. The kinematics are based on a parallel kinematic drive concept with three fixed motors that are mounted on a pyramid-shaped mechanical structure consisting of linear axes and carbon fibre-reinforced rods. The highly rigid mechanical design and low moving mass make the parallel kinematic system up to three times faster than comparable Cartesian systems. The robot is suspended from the top of the structure so that access to and usage of the workspace can be maximised, while also contributing to a reduction of the overall footprint.

FAQ about handling systems and robots

What are handling systems?

Handling systems are all devices that move an object towards a specific position and rotate it until it is in the correct position. They carry out functions similar to those of the human hand and have visual perception. Handling systems are therefore used for precise workpiece and tool positioning and are intended to relieve people of monotonous and physically heavy work. Handling technology replaces hands with tools, grippers, levers, holders and the like.

Handling technology plays an important part in manufacturing and assembly tasks, and its application is distinctly different from other applications. Handling is about more than just transporting a workpiece; it's about automatically moving or manipulating it. For example, when a workpiece needs to be turned, tilted or positioned.

Where are handling systems used?

Nowadays many manufacturing companies are forced to further optimise and automate their production processes because of growing competitive pressures and the ever increasing trend to automate production processes. That is why handling systems are used since they reduce error rates and increase production speed and efficiency. This primarily affects sectors such as machine building and the automotive industry, but also medical technology, the pharmaceutical industry and the electronics industry. The keys to greater efficiency, profitability, competitiveness and especially higher profits are maximum utilisation of machine running times, reduction of error rates and minimisation of unproductive downtime.