Electric Motion Sizing Release Notes
See what's new in Electric Motion Sizing and what we're gradually rolling out.
Release 02/2026
What's new
-
New stainless-steel motor: EMMH-AS
The new EMMH-AS motor series has been added to the database and is available in sizes 68, 88, 108 and 138.
The motor can be selected:
- For rotary applications and
- For linear applications in combination with the new EPRF axis.
-
New stainless-steel actuator: EPRF
The new EPRF axis series is now available for linear applications in sizes 36, 45, 55, 75 and 86.
EPRF axes do not include an external guide. To obtain valid results in EMS, the filter 'Calculate guide load' must be set to 'no' when selecting EPRF.
Bug fixes
- Removed unreleased ELGD variant
The axis variant ELGD-BS-KF-WD-100-...-20P-L has been removed from the database, as this version has not yet been officially released.
- Removed S3 controllers from selection
S3 controllers have been removed from the selection to simplify filtering and improve overall performance of the tool.
- Removal of mass moment of inertia calculator
The mass moment of inertia calculator has been removed, as it still belonged to the legacy xDKi platform. The corresponding servers will be shut down. The discussion for a suitable replacement is still ongoing.
Release 12/2025
What's new
-
ELGA now available for low-temperature environments down to -30 °C
ELGA axes are now suitable for applications in low-temperature environments down to –30 °C.
The axis can be selected by switching to "Roller guide".
When an ambient temperature below –10 °C is entered, EMS will automatically preselect the appropriate low-temperature ELGA variant.
-
Updated cable configurations for EMMT-EC, EMMT-ST and EMMB-ST
Cable specifications have been revised to ensure technical consistency and compliance:
- For EMMT-ST and EMMB-ST, the maximum cable length for part number 8181663 has been reduced from 25 m to 20 m.
- For EMMT-EC, four new cables have been added to the database and are now automatically selected based on the entered cable length:
- NEBM-M17G12-EH-2.5-Q9N-LE12
- NEBM-M17G12-EH-5-Q9N-LE12
- NEBM-M17G12-EH-7.5-Q9N-LE12
- NEBM-M17G12-EH-10-Q9N-LE12
-
New info button for slide filter
A new info button has been added to the slide filter, providing users with detailed insights on filter behavior and its effects on product selection.
Bug fixes
- Incorrect language displayed in MyFesto popup fixed
A defect that caused the MyFesto login popup to appear in the wrong language has been resolved. The popup now consistently reflects the user’s EMS language settings.
- Sorting options in Rack & Pinion applications restored
An issue preventing the sorting functionality from appearing in Rack & Pinion applications has been fixed. All sorting options are now visible and fully operational.
- Adjusted angular velocity calculation for rotary applications
The computation logic for angular velocity in rotary applications using a motion step table has been corrected to ensure accurate sizing results.
- Inactive filters for motion steps below 1 mm fixed
A bug that caused filters to become inactive when defining motion steps with target positions below 1 mm has been resolved. Filters now remain active and behave as expected in all precision ranges.
Release 10/2025
What's new
-
New save dialog for MyFesto integration
A redesigned save dialog has been introduced when saving projects to MyFesto.
-
Default mounting position for vertical applications:
For vertical applications, such as pressing, the mounting position is now automatically set to -90°.
Bug fixes
- Fixed typecodes for ELGD-TB-KF-WD-120
Typecodes for the ELGD-TB-KF-WD-120 has been corrected, ensuring valid configurations and orderability.
- Filtered out invalid 1-phase drive solutions with high-voltage motors
EMS will no longer suggest solutions that include 1-phase drives in combination with high-voltage motors.
- Restored missing ERMO versions with brakes
All ERMO variants equipped with brakes are now correctly listed again in the product database and sizing results.
- Broken info buttons repaired
Previously non-functional info buttons have been fixed and now properly display detailed parameter and product information as intended.
- Incorrect utilization values fixed
A display error that caused utilization values to appear above 100% has been resolved (visual bug).
- Pinion diameter handover for rack & pinion templates fixed
A missing filter caused a popup to appear, incorrectly prompting users to set the pinion diameter in rack & pinion application templates. The filter is now included in the initial query, preventing the unnecessary popup.
Release 09/2025
What's new
New actuators added
The following new actuator variants have been added to the system and are now available for selection and sizing:
- ELGD-BS-120
- ELGD-BS-120-WD
- ELGD-TB-120
- ELGD-BS-60/80/100WD with spindle support (-SU)
- ELGD-120-BS/BS-WD with spindle support (-SU)
Bug fixes
Missing drive combinations resolved:
Several actuator and motor combinations that were previously unavailable have now been added to the system:
- Fixed: Missing combination EGC-70-TB + EMGA-60-3:1 + EMMT-AS-60
- Fixed: Missing combination ELGD-100-WD-TB + EMMT-AS-60
- Several additional missing combinations were identified and resolved to improve completeness of available configuration options.
Release 07/2025
What's new
-
Default travel time set for motion steps
When adding new motion steps, a default travel time of 10 seconds is now automatically applied.
-
Rotary jerk value included in sizing report
The jerk parameter for rotary applications is now pasted into the motion step table of the sizing report, ensuring complete motion profile transparency.
-
Extended ELGD product range
Long-stroke ELGD axes are now available with stroke lengths of up to 8500 mm, expanding the applicability of the product family.
-
Updated database
The database has been updated, including new mounting kits and latest mechanical data.
Bug fixes
-
Economic sorting logic corrected
The sorting function for “most economic” solutions now works as intended, providing consistent and accurate result ordering in the solution list.
-
User-defined jerk field restored
A missing input field for user-defined jerk values has been fixed and is now displayed correctly when selecting this option in the advanced filter section.
Release 04/2025
What's new
- New motor types added
The EMMT-AS-...-40-... series has been integrated
- Jerk parameter for rotary load cases
The jerk value is now displayed for all rotary load cases, offering additional insight into motion dynamics.
- Improved nominal torque calculation
The calculation logic for the servo motors nominal torque has been optimized to improve precision.
Bug fixes
- Invalid combination removed
The incompatible combination of ELGD-TB-KF-WD-100 with the EAMM-A-T42-87-A axial kit has been removed to ensure valid sizing results.
- UI bug fixes
Various minor UI-related bugs have been resolved to enhance usability and ensure accurate data display.
Release 02/2025
What's new
- New Mounting Kits Available:
New mounting kits have been added. As part of this update, redundant parallel mounting kits have been removed to optimize the selection.
- ELGD Axis Now Supports Safe-for-Food Options:
The ELGD axes now support both Safe-for-Food and standard options:
- ELGD-BS: Suitable for both Safe-for-Food and standard applications
- ELGD-TB:
- PU1 - Safe-for-Food
- PU2 - Standard
- New Combinations Available
With the introduction of the new mounting kits, additional combinations are now possible, including:
- ELGD size 60 & EMMT-AS size 60
- EGC-HD size 160 & EMMT-AS-80
Bug fixes
- ERMO is now shown by default again (issue was caused by changes in the encoder selection).
- "Reset all filters" now works as expected.
- Max. support spacing is now displayed correctly in both the UI and PDF notifications.
- Filter dependencies for rotary applications now function correctly.
- Solutions no longer deviate from the user-specified stroke.
- Brake selection is now aligned with other application templates.
Release 12/2024
What's new
- Default encoder selection changed: The default value "Festo Recommendation" is now mapped with absolute single-turn encoders for the newly introduced stepper motor families EMMT-ST and EMMB-ST. The countries DE, AT and CH are an exception: Here, both stepper and servo motors will be displayed with absolute multi-turn encoders by default.
- Notification for manually added accessories: Accessories, which are manually added to the bill of materials of one selected solution, are not subject to any sizing calculation. It is important to check the applicability of such components with the specified application parameters before placing an order. This information is now added as notification into the tool UI and into the PDF sizing report.
- "Contact" form is now linked so that users can reach out to the Festo Technical Support in order to clarify questions related to a given solution. The contact form is automatically filled with a link to the specific Electric Motion Sizing project.
Bug fixes
- Fixed: Cantilever Axes ELCC have been filtered out too generously for applications with long stroke and high payloads.
- Fixed: Automatic motor brake selection has not worked properly in certain application cases with vertical mounting position.
Release 10/2024
What's new
- "Save solution" functionality: Users can save their individual solutions from Electric Motion Sizing in the newly introduced MyFesto cloud platform in order to create and collaborate on their project BoM. This functionality requires an "Express Account" on www.festo.com, which is being created within just a minute.
- "Target position" input for rotative applications ("General linear load case") is changed from relative [no. of rotations] to absolute [°]
- Toggle button +/- added to the parameter input "External torque"
- "Actuator support spacing" added as input parameter, exclusively affecting solutions with the linear actuator ELGD. This parameter can be used for specifying applications in which a long axis stroke may cause deflections of the axis.
Bug fixes
- Fixed: Electric Motion Sizing displayed invalid solutions from the cache in certain cases. Users can easily check, if their project/solution was affected, by reopening the solution from the link in the downloaded PDF sizing report. If the solution is displayed again upon reopening, then it is not affected.
- Fixed: Adobe Reader was not able to properly save the URL of an EMS solution within the PDF sizing report in certain cases. Reopening such solutions from Adobe Reader therefore caused problems in these cases. The URLs are now being compressed for Adobe Reader in order to avoid this behavior.
- Fixed: The PDF sizing report did not update with minor modifications to a selected solution, e.g. selecting a PLC type or adding project data.
- Fixed: Configurable options of EGSK (H-class, P-class, short slide) are removed from the tool's product scope.
- Fixed: Suitable motor cables have not been automatically added to solutions with stepper motors EMMB-ST and EMMT-ST with motor brake
Release 07/2024
What's new
- New stepper motor families EMMT-ST and EMMB-ST are added to the tool
- the "old" stepper motor family EMMS-ST is removed from the default selection. If needed, it can be manually selected in the "Motor family" filter.
- Speed-torque extension of the operating range by using the field weakening mode for the EMMB/T-ST motors
- Permitted operation of EMMB/T-ST motors in the overload range with consideration of i²t for continuous operation
- Phase-out process of servo motor family EMME-AS with flange sizes 60, 80 and 100 has started. These motors are no longer available in the tool.
- The former "Multi-Position-Handling" entry pages are renamed to "General linear load case" and "General rotary load case"
- Automatic renaming of PDF sizing report: If users enter project data before downloading the PDF report of a given solution, these data will be used for the name of the download file
- The servo drive family CMMP-AS is removed from the default selection in order to improve the overall tool performance.
- Improved usability when applying filter changes: The pre-filtering calculation process is now done without causing a completely blocked screen after every click event in the product filters. Instead, a loading spinner in the footer indicates that the pre-filtering is running.
- Improved compatibility of old URLs (e.g. links from previously downloaded PDF sizing reports) with updated software versions.
Bug fixes
- Fixed: the entered pause time after every motion step was ignored in the sizing calculation in certain edge cases.
- Fixed: accessories for ball screw axis ELGD-BS where not accessible in certain countries.
- Fixed: Stroke length was not displayed in the type code of external guide units EAGF.
Release 03/2024
What's new
- New CMMT-AS servo drives in the power classes 9kW and 12kW are added to the tool.
Release 02/2024
What's new
- New template for Festo drive with user-defined transmission
- Possibility to define center of force (X, Y, Z) is added to the tool
- Workloads >90% are no longer highlighted in yellow colour. Why? The tool includes an algorithm that optimizes every solution "as fast as possible" by default. In most cases this leads to at least one component of a solution being utilized to its limit (99%). This does not mean that this solution is at its absolute limit for the given application parameters - in most cases it can easily do the application with lower workload just by not running as fast as possible.
- New axis ELGD added as "long slide" versions
Bug fixes
- Fixed: Description of "Nominal torque" and "RMS torque" was mixed up in the "motor characteristics" section.
Release 01/2024
What's new
- New ball screw and toothed belt axes ELGD-TB and ELGD-BS added to the tool. The toothed belt type ELGD-TB is available with sizes 60, 80 and 100-WD, the ball screw type ELGD-BS with sizes 80 and 100-WD. More sizes and options will follow in the upcoming months.
- The term "jerk" is added to the input parameter "acceleration behavior" in order to highlight that this input has an indirect or - by using the optional input "user-specific jerk" - direct effect on the jerk value in the motion profile.
- The info button text for the input parameter "Mass moment of inertia ratio" now includes the information about how the selected values are applied to servo and stepper motors respectively.
Bug fixes
- Fixed: Automatic motor cable selection for combinations CMMT-AS servo drive with EMMT-AS servo motor has been updated according to the selection logic as described in the EMMT-AS catalogue.
- Fixed: Solutions with extra low voltage drive CMMT-ST-MP have not been displayed when selecting Modbus TCP as fieldbus.
Release 11/2023
What's new
- Additional input option "user-defined jerk" [m/s³; rpm/s²] is now added to the filter "Acceleration behavior". The new input allows users to define the jerk, which is then applied to acceleration and deceleration of all steps of the motion cycle, themselves.
- New servo motors EMMT-AS-100 with length "very long" ("-H-") added to Electric Motion Sizing.
- User can now easily navigate one page back using the "back" button on the top left.
- Image added to the load case "Conveyor" in order to highlight the fact that the input parameter "Total inertia of all rollers" requires to consider both drive and idler rollers.
- Calculated value "required usable force [N]" added to the displayed results parameters.
- Info button added to give more explanation about the "Festo recommended" encoder type. The default settings (="Festo recommendation") go for an absoulute multi-turn encoder for all servo motor product families (EMMT-AS, EMMB-AS, EMME-AS) and for an incremental encoder for the stepper motor family EMMS-ST.
Info button added in order to give additional explanation to the input field "Mass moment of inertia" within the "Index table" load case template.
Bug fixes
- Fixed: For the load case "Index Table" the calculation results have been partly displayed wrongly as the transmission ratio of the user-defined non-Festo transmission mechanism was not considered. This bug has not had an effect on the actual sizing calculations, in which the transmission ratio has been considered correctly. I.e. all displayed results have been valid based on sizing calculations.
- Fixed: It is now possible to use more characters for adding project data to the sizing report PDF.
Release 10/2023 (hotfix)
Bug fixes
- Fixed: Transmission ratio of Non-Festo transmission mechanism has not been considered for the displayed calculation results speed/acceleration/jerk/emergency
stop. This bug affected exclusively the Index Table load case. The actual sizing calculations have considered the transmission ratio, i.e. all
displayed/selectable results have been calculated correctly and have therefore been valid.
Release 08/2023
What's new
- Add project data to documentation: Users are now able to add project specific information to the sizing report PDF for documentation purposes. The information can be added in a popup window when starting the sizing report download. This is an optional input, i.e. the download can also be startet without adding project data. The inputs from users are not being saved.
- Additional explanation added to the filters "Guide type" and "Motor brake" about what "Festo recommendation" means.
Bug fixes
- Fixed: EGC axes with heavy duty guide (EGC-HD) have not been included into the tool as versions with protected slide
- Fixed: Workloads of rotary modules ERMO & ERMB have been calculated not considering the internal transmission of the actuators (only a bug in the displayed value, no bug in the actual sizing calculation, i.e. displayed solutions are still valid)
Release 07/2023
What's new
- Automatic selection of braking resistors: For solutions with servo motors the tool has indicated the demand for an external braking resistor, if needed, for quite a while. Now it automatically selects a suitable braking resistor from our catalogue based on nominal power and resistance value as selection criteria. If multiple braking resistors are suitable, then the one with the smallest nominal power (i.e. the one with the lowest list price) will be selected. If no suitable resistor can be found in our portfolio, then only the notification text will be displayed to users.
- Electrical slide EGSK added to actuator selection. Users can now select EGSK for applications that require both high repetition accuracy and high rigidity.
- Default encoder selection for servo motors changed to "absolute multi-turn": The definition of "Festo recommendation" is now changed, so that for solutions with servo motors the tool will propose the absolute multi-turn encoder versions instead of single-turn.
- The calculated jerk value [m/s³] is now printed into the motion profile table in the sizing report PDF.
Bug fixes
- Fixed: The requested input value "roll inertia" (template: Conveyor Belt) is renamed to "total inertia of all rolls".
- Fixed: Input value "Mass moment of inertia" was converted wrongly in the sizing report PDF for the "Index Table" template.
Release 06/2023
What's new
- New product CMMT-ST with multiprotocol option (PROFINET, EtherCAT, EtherNet/IP, Modbus TCP) added to the tool. At the same time, the "old" CMMT-ST versions with dedicated fieldbus interfaces (part numbers 8084004, 8084005 and 8084006) are removed from Electric Motion Sizing.
- Link to Mass Moment of Inertia calculator: Whenever the user is asked to define an application's mass moment of inertia, the tool now offers a calculator where users are assisted calculating the correpsonding inertia.
Bug fixes
- Fixed: Selection criteria for automatically adding an external guide EAGF to electric cylinders (ESBF, EPCC) depending on payload, mounting position and center of gravity of mass have been modified.
- Fixed: Users can now define negative ambient temperatures.
- Fixed: Users can now define 3rd party transmission ratios in decimal number format.
Release 05/2023 (Part II)
What's new
- Notification added to the motor characteristics curve: "The displayed motor characteristics apply for the selected combination of motor and servo drive. It may therefore deviate from the "ideal" motor characteristic curve as shown in the catalogue."
- Automatic motor cable selection for the following motor types: EMMT-AS-150-L-HS-..., EMMT-AS-150-L-HT-..., EMMT-AS-190-...
- Info button for "Transmission ratio" (3rd party transmission): "Transmission acts reducing, i.e. the higher the transmission ratio the higher the required motor revolution."
Bug fixes
- Fixed: Invalid (i.e. overloaded) solutions have been displayed in cases where users have defined an exact travel time ("=") and a specific speed or acceleration/deceleration.
- Fixed: Problems reopening a copied URL with solutions with rotary modules ERMO & ERMB.
- Fixed: Negative values can no longer be put into the motion step table for the parameter "External Torque" (in cases where the sign is defined by a +/- toggle button).
Release 05/2023 (Part I)
What's new
- Functionality of the "Connectivity Finder" tool is now integrated
into Electric Motion Sizing. This way, users will have easy access to all available expert knowledge that helps connecting the selected Festo servo drive
to their preferred PLC. The corresponding links to all available expert knowledge will also be saved in the sizing report
PDF.
- Users are now able to define their preferred actuator stroke independent from the max. stroke of the
application.
Bug fixes
- Fixed: Calculation of max. torque Mx on actuator guide has not been calculated correctly in random/rare cases with a defined radial mounting orientation of
90° (slider sideways).
- Fixed: Result parameters for load cases with Non-Festo kinematics (Rack & Pinion, Conveyor Belt, Ball Screw Actuator) are now displayed in linear units
- Fixed: There used to be a tolerance of 0,5p.p. for the calculated guide workload, which lead to results with 101% guide load. This tolerance is now removed
so that no solutions with workloads higher than 100% are displayed.
Release 04/2023
What's new
- Sizing of motors and drives for Non-Festo kinematics: Index Table, Conveyor Belt and Ball Screw Actuator are added as load
cases.
- The "reset filters" function now exclusively effects the filters. The defined motion profile will remain as defined by the
user.
- All CMMP-AS-...-M3 servo drives are now selectable
- EMGC gearboxes removed from selection (due to EMCA and EMGC being in phase-out process)
- "No selection" value is moved to the top of the list within the "Supply Voltage" filters
- Linear axis ELGR removed from default selection for US, CA and MX
Bug fixes
- Fixed: Wrong parameter name "Ball screw inertia" in Rack & Pinion template
Release 02/2023 (Part II)
What's new
- Phased out products (EMCA and EPCO) have been removed.
- The EPCC-..-KF variants have been added.
Bug fixes
- Fixed: Wrong filter combination leads to incorrect update of possible solutions.
- Fixed: Rack & Pinion wrong sign calculation leading to incorrect torque values.
- Fixed: 'Actuator family'-Filter is now hidden correctly, when user specific rotary template is used.
- Fixed: When calculation of guide load is deselected, the 'Guide workload' is now hidden in the results.
- Fixed: 'Max. Jerk' has been added to the PDF-Report.
Release 02/2023 (Part I)
What's new
- Sizing of motors and drives for Non-Festo kinematics: Rack & Pinion is added as first template for simple calculation of typical load cases. Additional
templates for Index Table, Conveyor Belt and Spindle Actuator will follow in the upcoming releases.
- New filter for acceleration behaviour: Users are now able to define the dynamics of acceleration and deceleration by setting the desired behaviour. A "
soft" acceleration behaviour, as example, will set the acceleration time to 100ms, which will eventually lead to a relatively low jerk (m/s³) in the motion
profile. A "hard" acceleration, on the other hand, leads to a relatively high jerk up to max.
1500m/s³.
- New filter for repetition accuracy: It is now possible specifically filter down to "precise" actuators with a repetition accuracy of 0,02mm and
better.
- EMMT-AS motors can now be calculated with a supply voltage up to 480V AC.
- Duty ratio of external braking resistor is displayed as result parameter (duty ratio is shown as %-value with total cycle time as reference)
- Max. Jerk is displayed as result parameter.
- All filters are now added to all entry pages ("show advanced filters").
Bug fixes
- Fixed: Maximum actuator workload was displayed incorrectly (since release 2022-12)
- Fixed: Texts were displayed in white colour on white background on iPhone/iPad
- Fixed: Animations started automatically in fullscreen on iPhone/iPad
- Fixed: solutions are no longer filtered out based on mass moment inertia ratio for movement type "Acceleration and continuous operation"
Release 12/2022
What's new
- Workload calculation of each component is now differentiating between effective and maximum workload (same like it used to be in PositioningDrives).
- "Regulation loop" filter is renamed to "Mass moment of inertia ratio" in order to avoid misunderstandings.
- Maximum number of motion steps that can be defined is increased from 5 to 20 in order to allow definition of more complex motion profiles.
- Gantry axis ELGT is removed from the default selection for USA and Canada.
Release 10/2022 (Part II)
Bug fixes
- Fixed: Titles and subtitles were not translated correctly
- Fixed: Combinations rotary module ERMB + gearboxes were excluded from the tool
- Fixed: General bugs with newly introduced dynamic filter dependencies
- Fixed: Motor curve was not displayed in the PDF sizing report
- Fixed: Sign of external forces was not transferred correctly into the PDF sizing report
- Fixed: Info button content for product families was incomplete or empty
- Fixed: Criteria for automatic selection of external guide unit EAGF for electric cylinders ESBF were incomplete
Release 10/2022 (Part I)
What's new
-
Sign logic for external forces is changed again (back to old logic): A positive force acts accelerating in the direction of movement, a negative force acts decelerating in the direction of movement.
-
Dynamic filter feedback: The selection filters have an improved behaviour so that the impact of changes in one filter to another filter become more visible.
-
Show all solutions: Users are now able to decide wether the tool should show recommended solutions only (like it used to be until now) or whether all possible and valid combinations based on a certain selection should be displayed.
-
Highlight and share 1 selected solution: It is now possible to highlight a selected solution in the solution list. When sharing the URL of a sizing project with one selected solution then this solution will still be selected and highlighted when re-opening this project (URL).
-
Apply filters: Filter modifications are no longer applied immediately. Instead, users can modify multiple filter selections at once and trigger a new calculation by pressing the "Show results" button
-
Acceleration curve added to motion profile graph
-
Additional Information for product families: The info buttons for "Servo drive family", "Motor family" and "Actuator family" now give additional information to users about the different families offered by Festo
Bug fixes
- Fixed: Calculated values "Displacement during emergency stop" and "Deceleration for emergency stop" have been displayed in the wrong unit.
- Fixed: Unit "s" for "Travel time" was not shown in the motion step table.
Release 06/2022 (Part II)
Bug fixes
- Fixed: Size selection for integrated actuators EPCO and ERMO.
- Fixed: Entering 0 value as the target position in the rotary motion profile will no longer be accepted.
Release 06/2022 (Part I)
What's new
-
Motor brake filter added: It is now possible to manually select/deselect a motor brake regardless of the Festo recommendation. The default value for this
filter remains "Festo recommendation", which means that a motor brake will automatically be added as soon as the application parameters require to do so.
-
Service life notification: Whenever the calculated expected ball screw service life is 1000km or less, a notification will be shown to the user in the
solution overview.
-
Stepper drive CMMO-ST removed from Electric Motion Sizing: The product is in phase-out process and therefore no longer available in the tool.
Bug fixes
- Fixed: Info button image "Center of gravity of mass" was too small.
- Fixed: Linear actuator ELGR was displayed as rotary actuator family.
- Fixed: Actuator sizes of linear actuators were displayed in the rotary section.
Release 05/2022 (Part II)
What's new
-
New servo motors EMMT-AS sizes 150 and 190 added to Electric Motion Sizing. The new motors as well as the compatible cables and mounting kits are now included into the solutions offered by the tool.
-
Mounting position can now be freely defined between -360° and +360°.
-
Solutions with stepper motors are no longer automatically calculated with 48VDC in cases when the default supply voltage 24VDC delivers 0 solutions. Instead, the user will be notified and guided to starting a new calculation with 48VDC supply voltage.
-
Title of PDF download is changed from "fact sheet" to "sizing report"
Bug fixes
- Fixed: Control options/fieldbusses where not assigned correctly to the motor controller families CMMP-AS and CMMO-ST (since release 05/2022 Part I)
- Fixed: Servo drive and actuator filter clusters used to swap their positions randomly when applying changes to the filters.
- Fixed: Integrated motors EMCA got "lost" during the last release 05/2022 (Part I)
Release 05/2022 (Part I)
What's new
-
CMMT-AS Multiprotocol: The new CMMT-AS devices with multiprotocol functionality (all 3 fieldbusses PROFINET, EtherCAT and EthernetIP integrated into 1 device) are now included into Electric Motion Sizing. These new devices are replacing the CMMT-AS servo drives with 1 part number for each fieldbus.
-
Fine filtering option for gear ratio: Users can now filter down the results according to their preferred gear ratio(s).
-
Fine filtering option for motor size: Users can now filter down the results according to their preferred motor size(s).
-
Fine filtering option for actuator size: Users can now filter down the results according to their prefererd actuator size(s).
Release 03/2022
What's new
-
New servo motor EMMT-AS size 150 added: Our servo motor family EMMT-AS is now extended with flange size 150. These new motors will be shown as results if
the application parameters require size 150 and the corresponding power.
-
Motor characteristics curve: Users are now able to see the motor characteristic of every solution based on the individually calculated motion
profiles.
-
Pressing application template: A new template is added so that users can now easily find solutions for their press-fitting
applications.
-
Cantilever axis template: With this new template it is possible to easily find solutions for z-axes using cantilever
actuators.
-
Copy bill of materials to clipboard: It is now possible to copy the BoM to the clipboard so that it can be pasted into various other applications and
documents.
Bug fixes
- Fixed: Wrong motor cables were added to the bill of materials for combinations of servo drive CMMP-AS and servo motor EMMT-AS.
- Fixed: Link to Handling Guide Online did not work in certain countries.
Release 02/2022
What's new
-
Sign logic for external forces has changed: Due to inconsistency with other tools, it is necessary to change the logic how external forces can be defined
in Electric Motion Sizing.
- old logic: A positive force acts accelerating in the direction of movement, a negative force acts decelerating in the direction of movement.
- new logic: The coordinate system is our reference! A positive force acts into positive X-direction, a negative force acts against positive X-direction.
This means that a continuously acting force against positive X-direction will act decelerating when extracting (i.e. moving in positive X-direction) and
accelerating when retracting.
-
Complete UI redesign: The appearance of Electric Motion Sizing was subject to a complete makeover. It now comes with several improvements based on user
feedback that was collected during the past months.
Important note: As several substantial changes have been made, the tool can not handle URLs of the "old" design any more.
-
Filters added to application templates: Users can now specify the two filters "Fieldbus/Control" and "Actuator Type" already before doing the first
calculation. These filters are implemented into the different application templates.
-
Advanced filtering mode: When using the motion step table for defining the motion cycle in detail, users can now access the entire range of filters
before running the first calculation. This saves time for users who have very specific requirements towards the
solution.
-
Numbering of results: For a better overview, the listed results are now coming with numbers that users can refer to when collaborating on a sizing
project.
Bug fixes
- Fixed: Wrong part numbers were shown in the PDF fact sheet for ESBF cylinders with external guides EAGF.
- Fixed: Actuator masses now completely bypassed for horizontal and vertical mounting positions when the guide load should not be considered (external guidance
required)
- Fixed: Acceleration filters outgoing from mounting kit, motor and actuator for rotary applications including rotary modules (ERMO, ERMB) consider all
technical parameters now
Release 11/2021 (Part II)
What's new
- Download commissioning file: Users can now download the commissioning file for easy import in Festo Automation
Suite
Bug fixes
- Fixed: Missing EMGC gears are now shown together with integrated motors EMCA.
Release 11/2021 (Part I)
What's new
- Results sorting: Users can now sort the shown results by price (default), by cycle time and by mass moment of inertia
ratio.
- New ball screw linear actuator ELGT included in Electric Motion Sizing. Please note that certain functionality is still reduced as long as the online
catalogue is not yet updated with ELGT: No product image, no accessories selectable. However, it is possible to order ELGT via the online shop.
- Integrated drive EMCA included. EMCA is handled as motor family in the tool and is deselected by default.
- Integrated electric cylinder EPCO included. EPCO is deselected by default.
- Default ambient temperature is changed from 25°C to 20°C (in order to be conform with other Festo engineering tools)
Bug fixes
- Fixed: Comma-inputs were ignored when using the slider direct input field (for certain language versions).
- Fixed: Motion profile graph used to not "use" the entire x-axis.
- Fixed: Breadcrumb menu navigation for standalone version (for countries where the new Festo website is not yet rolled out) used to disappear in certain
cases.
- Fixed: Entered values in edit fields could not be deleted, only changed.
- Fixed: The entire tool header for standalone version (for countries where the new Festo website is not yet rolled out) used to link to the starting page,
losing all entered and changed parameters. Now only the Festo logo in the header links to the starting page.
Release 09/2021
What's new
- Release Notes: From now on releases of Electric Motion Sizing will be documented in this Release Notes page. This page can be accessed internally as well
as externally. Important: Release Notes are only available in English language:
https://www.festo.com/eac/en-us_us/ReleaseNotes/electric-motion-sizing/
- Regionalization of default values: Default values can now be defined on country-level. Regional variations of default values have been implemented for
servo motor family (EMMB-AS), power supply (120V in US, CA, MX) and fieldbus selection.
- Gantry axis ELGR added:
- Motor family EMME-AS added:
- "Guide type" filter added: Users can now manually select the preferred guide technology for linear
actuators.
- Filter for mass moment of inertia ratio added: The filter "regulation loop" offers the 3 options "dynamic", "standard" and "soft". These 3 options stand
for three different upper limits of mass moment of inertia ratio.
- Filter dependencies are now implemented: For certain filters, user selections have an impact on possible values of other filters. These dependencies are
now implemented for:
- Motor Technology - Motor Family
- Fieldbus/Control - Servo Drive Family
- Actuator Type - Actuator Technology - Guide Type - Actuator Family
- Improved info button for "center of gravity of mass": The info button image now shows the coordinate system for 3 different mounting orientations.
- Travel times of individual steps in the motion profile are now listed in the calculation results.
- Supply voltage is now shown as value in the calculation results. The nominal voltage of the selected component is not displayed anymore in order to avoid
confusion.
Bug fixes
- Logic for adding external guide unit EAGF to electric cylinders ESBF has been modified. EAGF will be automatically added to electric cylinders ESBF
according to the following logic:
- for horizontal orientation if the moving mass is > 0kg
- for vertical orientation if the moving mass is > 0kg and the center of gravity of mass is not 0/0/0
- in all cases, EAGF will only be added if the user selects "Consider effect of load on the actuator guide"
- Motor shaft filter fixed. Users can now select either smooth output shaft or feather key shaft (to DIN 6885) for rotary applications.
- PDF report download works reliably again.
Release 08/2021
What's new
- Improved filtering algorithm: "Quality" (competitiveness, comparability with PositioningDrives) of displayed results. Less cases of highly
overdimensioned results or 0 results.
- Encoder selection filter changed to single-select: Users can now select 1 encoder type. Global default value is "FESTO Recommendation", which stands for
single-turn encoder (servo motors) and incremental encoder (stepper motors).
- Local language versions: Electric Motion Sizing is now fully translated for China, Hongkong and Taiwan
Bug fixes
- "Non-standard" configurable variants are filtered out: The tool used to display non-standard variants, like EGC-TB with proximity sensor ("-Z"), for no
particular reason. These are now being filtered out.
- Sizing of cantilever axes ELCC now works properly. Still, users need to change the "actuator type" filter selection from "Gantry axis" (default) to "
Cantilever axis".
- Negative input values for Center of Gravity of Mass (X/Y/Z) is now possible.
Release 06/2021
What's new
- Improved sharing functionality: URL can be copied to clipboard by clicking "Share" icon on the top right
- Local language versions: Electric Motion Sizing is now (partly) translated to local languages
- translation is almost complete for some countries
- for other countries, only parts of the texts are translated into local language, others are still in EN
- translation process will continue, upcoming releases will have more and more local language content
Bug fixes
- ERMO removed from selection: since ERMO is currently not yet implemented into Electric Motion Sizing, the respective value has been removed from the "
actuator family" filter
- All input parameters are now written into URL: Information for center of gravity of mass as well as for max/exact travel time got lost when copying and
pasting URL to a new browser window.
- Accessories available also for non-FoX countries: Accessories can now be selected and added to the bill of materials, also for countries where FoX is not
yet rolled out.
Release 03/2021
What's new
- Welcome to our first release of Electric Motion Sizing You can use the URL https://www.festo.com/ems>to access the application from everywhere
globally.