Title:
How to setup „Travel to fixed stop“ with CMMT-AS-PN by using the SINA_POS / telegram 111
Subtitle:
CMMT-AS-...PN
Description:

This document describes how to set up the CMMT-AS-...-PN in "trav-el to fixed stop" mode by using the SINA_POS function block / telegram 111 in programming environment of TIA Portal

Document type:
Application Note
Title Version
Application Note - How to setup „Travel to fixed stop" with CMMT-AS-PN by using the SINA_POS / telegram 111

This document describes how to set up the CMMT-AS-...-PN in "trav-el to fixed stop" mode by using the SINA_POS function block / telegram 111 in programming environment of TIA Portal

如何使用 SINA_POS/报文 111 设置 CMMT-AS-PN 的“行进到固定挡块”

本文档介绍如何在“行进到固定挡块”模式下使用 SINA_POS 功 能块/报文 111 在 TIA Portal 编程环境中设置 CMMT-AS-...-PN。