Title:
Festo Maintenance Tool with Rockwell RSLogix 5000 L5K file Export/Import
Subtitle:
CPX-FB32; CPX-FB36;Rockwell; RSLogix 5000
Description:

This document provides procedures to use the FMT (Festo Mainte-nance Tool Software) to export a "*.L5K" Rockwell Automation file. This file is then imported by RSLogix 5000/Logix Designer 5000 Rockwell Automation Software. The import creates a GENERIC ETHERNET-MODULE used as a EtherNet/IP connection to the device configured in the FMT (Festo Maintenance Tool Software).

Document type:
Application Note
Title Version

Application Note - Festo Maintenance Tool with Rockwell RSLogix 5000 L5K file Export/Import

 

This document provides procedures to use the FMT (Festo Mainte-nance Tool Software) to export a "*.L5K" Rockwell Automation file. This file is then imported by RSLogix 5000/Logix Designer 5000 Rockwell Automation Software. The import creates a GENERIC ETHERNET-MODULE used as a EtherNet/IP connection to the device configured in the FMT (Festo Maintenance Tool Software).