Title:
CMMT-AS Parallel Axis Synchronous Position Absolute
Subtitle:
CMMT-AS Parallel Axis Synchronous Position Absolute
Description:

When 2 physical axes are rigidly coupled together by the load or other means (examples: gantry system X/X' coupled by a Y-Axis or 2 x ESBF rods attached), then it is necessary to synchronise/Gear these axes with an electronic alignment (Master to Slave).

 

This application note discusses the required settings to control the 2 x parallel linear axes in Synchronous Position Absolute mode using CMMT-AS-xx controllers.

It also discusses ways to implement monitoring of Slave faults and
Error situations based on the “Cross wire monitoring”

Any PLC could be used for the control. Rockwell is just an example.

Document type:
Application Note
Title Version
CMMT-AS Parallel Axis Synchronous Position Absolute

When 2 physical axes are rigidly coupled together by the load or other means (examples: gantry system X/X' coupled by a Y-Axis or 2 x ESBF rods attached), then it is necessary to synchronise/Gear these axes with an electronic alignment (Master to Slave).

 

This application note discusses the required settings to control the 2 x parallel linear axes in Synchronous Position Absolute mode using CMMT-AS-xx controllers.

It also discusses ways to implement monitoring of Slave faults and
Error situations based on the “Cross wire monitoring”

Any PLC could be used for the control. Rockwell is just an example.

CMMT-AS 平行轴 绝对同步位置

当 2 个物理轴通过载荷或其他方式刚性耦合在一起时(示例:通过 Y 轴或 2 个连接的 ESBF 连杆耦合的门架系统 X/X'),需要通过电子 对齐(主轴到从轴)同步/驱动这些轴。 本应用说明介绍使用 CMMT-AS-xx 控制器在绝对同步位置模式下控制 2 个平行直线驱动轴所需的设置。 还介绍了如何根据“交叉电线监测”监测从轴故障和错误情况。 可使用任何 PLC 进行控制,其中包括 Rockwell。