Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202207 - Security Advisory - CPX-CEC-C1 and CPX-CMXX, Missing Authentication for Critical Webpage Function Missing Authentication for Critical Webpage Function

Unauthenticated access to critical webpage functions (e.g. reboot) may cause a denial of service ofthe device.

1.1.1
FSA-202208 - Security Advisory - Unsafe default Codesys configuration Multiple Festo products contain an unsafe default Codesys configuration

The products are shipped with an unsafe configuration of the integrated CODESYS Runtime environment. In this case no default password is set to the CODESYS PLC and therefore access without authentication is possible.

 

With a successful established connection to the CODESYS Runtime the PLC-Browser commands are available. Thus granting the possibilities to e.g. read and modify the configuration file(s), start/stop the application and reboot the device.

1.0.1
FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
FSA-202401 - Security Advisory - Several Codesys Vulnerabilities in Festo Products

Several high severity vulnerabilities in CODESYS V3 affecting Festo products could lead to Remote Code Execution or Denial of Service.

1.0.0
Boot Application loading without CoDeSys V3.5 CECC; CPX-CEC (V3)

A brief explanation on how to load a new project to a Festo PLC over Ethernet without the use of the CoDeSys 3.5 software

1.10
05/07/2016
CANopen in CODESYS V3 CODESYS V3, CPX-FB14, CTEU-CO, CMMP-...-M0/M3, EMCA-CO

This document describes what each CAN parameter in the CODESYS V3 programming environment does, as well as show the available Function Blocks to implement diagnostics or pa-rameterization within the PLC’s Task.

 

 

 

1.10
04/08/2017
CODESYS OPC DA server CODESYS Development System >= V3.5 SP12

This application note describes the license dependency with the CODESYS OPC DA server and possible alternatives for CODESYS Development System >= V3.5 SP12

1.20
22/07/2020
CODESYS SOFTMOTION + example program CPX-CEC-M1-V3; CMMP-AS-…M3/M0; CODESYS SoftMotion

This Application Note is a collection of functions, parameterisa-tions and any supporting issue around CODEYS SOFTMOTION and FESTO drives. It is going to modified and complemented continuously.. Finally published with different versions of this Application Note.

The given single topics in this Application Note are not at all sorted by any specific sequence. It is a good idea to use the Windows search function.

1.10
06/10/2017
Commissioning of CPX-FB36 ModbusTCP with Schneider M580 CPX-FB36, Schneider M580

The application node contains a step by step explanation how to configure and handle a CPX-FB36 in Modbus/TCP mode with a Schneider M580 PLC and Unit Pro L V11.0

1.10
20/10/2016
Commissioning of CPX-FB40 with Automation Studio CPX-FB40, X20 CP 1585

The application node contains a step by step explanation how to configure a CPX-FB40 Ethernet POWERLINK valve terminal via B&R Automation Studio Software.

1.10
12/05/2016
Commissioning of SDAT in I-Port mode with CPX-CTEL-...-LK SDAT; CPX-CTEL

The application node contains a step by step explanation how to configure a SDAT-MHS-M100-1L-SA-E-0.3-M8 in I-Port mode with CPX-CTEL-2-M12-5POL-LK and Codesys V3.5 pbF

1.10
28/03/2017
CPX-FB36 EtherNet/IP to Micrologix1400 CPX-FB36; CPX Terminal; Micrologix1400; RSLogix 500; Example project included

Festo CPX-FB36 communication to Allen Bradley MicroLogix1400 PLC

The CPX-FB36 bus node is used as part of a CPX terminal and for communication as a participant in networks with the protocol EtherNet/IP.

This document has information combined from multiple resources for the intention of reducing the effort of a user who is configuring this application type.

1.10
27/11/2019
CPX-FB36 in Ethernet/IP Mode with a Schneider M340 CPX-FB36; Schneider M340 PLC; Unit Pro S 13.0

The application node contains a step by step explanation how to

configure and handle a CPX-FB36 in Ethernet/IP mode with a

Schneider M340 PLC and Unit Pro S 13.0

1.10
16/01/2019
CPX-FB36 Integration with Emerson DeltaV using Modbus TCP CPX-FB36 Integration with Emerson DeltaV using Modbus TCP; Library included

This Application Note explain the Festo CPX-FB36 (Slave/Server) ModbusTCP communication to Emerson DeltaV (Master/Client) The CPX-FB36 bus node is used as part of a CPX terminal.

1.10
26/03/2024
CPX-FB36 Modbus TCP Slave/Server to Micrologix1400 Master/Client CPX-FB36; Micrologix1400; Example project included

Festo CPX-FB36 (Slave/Server) ModbusTCP communication to Allen Bradley MicroLogix1400 PLC (Master/Client). The CPX-FB36 bus node is used as part of a CPX terminal and for communi-cation as a participant in networks with the protocol ModbusTCP. This document has information combined from multiple resources for the in-tention of reducing the effort of a user who is configuring this application type.

1.10
08/07/2020
CPX-HART module configuration with Portal TIA and PROFINET CPX-4AE-4AA-H

How to configure CPX-4AE-4AA-H module using Siemens TIA Portal® with PROFINET.

1.10
24/09/2018
CPX-HART with Rockwell Logix and EtherNet/IP + CMSH CPX-P; CPX-HART; CPX-FB36

How to make best use of the CPX-HART modules when using
EtherNet/IP in a Rockwell Logix environment. This includes a
Festo AOI, FTD/DTM, plus visualization tools from
PlantPAx using FactoryTalk View.

1.20
25/08/2022
CPX-IOT with EtherCAT CPX-IOT with EtherCAT

This document describes how to set up a CPX-IOT gateway and how to use
all the performances of the device in EtherCAT environment.

1.10
21/12/2021
CPX-IOT with EtherNet/IP CPX-IOT with EtherNet/IP

This document describes how to set up a CPX-IOT gateway and how to
use all the performances of the device in EtherNet/IP environment.

1.10
21/12/2021
CPX-IOT with PROFINET CPX-IOT with PROFINET

This document describes how to set up a CPX-IOT gateway and how
to use all the performances of the device with PROFINET environment.

1.10
21/12/2021
Driver Block Library for PCS7 Driver Block Library for PCS7

Commissioning devices using the PCS7 driver library- for CTEU and CPX Bus Nodes.

1.10
19/01/2026
Electronic CAM - SOFTMOTION CMMP-AS-…M3/M0; CPX-CEC-M1-V3

Step by step description how to set up an Electronic CAM pro-ject in CODESYS V3.5

1.10
08/03/2017
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
EtherNet/IP IO-Link Integration CTEU-EP, CPX-FB36, CPX-CTEL-LK

Controlling IO-Link Devices with Festo EtherNet/IP Products

1.30
28/07/2016
Festo CPX and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects CPX-FB36 and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects

How to extract data from CPX-FB36 systems using the built-in auto-discovery feature of Factory Talk Edge Gateway by Rockwell Automation.  What are the use cases of this data, and how to supplement it by using Factory Talk Smart Objects.

1.10
06/12/2022
Festo CPX-FB36 with Rockwell PLC and Safety Module Application Notes Festo CPX-FB36 with Rockwell PLC and Safety Module Application Notes

This application note explains how to control a VTSA valve terminal with the field bus node CPX-FB36 in a Rockwell safety module environment.

1.10
08/01/2024
Festo Maintenance Tool with Rockwell RSLogix 5000 L5K file Export/Import CPX-FB32; CPX-FB36;Rockwell; RSLogix 5000

This document provides procedures to use the FMT (Festo Mainte-nance Tool Software) to export a "*.L5K" Rockwell Automation file. This file is then imported by RSLogix 5000/Logix Designer 5000 Rockwell Automation Software. The import creates a GENERIC ETHERNET-MODULE used as a EtherNet/IP connection to the device configured in the FMT (Festo Maintenance Tool Software).

1.10
17/08/2019
How to mount SMB (CIFS) share CECC-…; CPX-CEC-...-V3 , CPX-E-CEC

This application note describes how to establish a SMB (CIFS) share with Festo PLCs CECC-.. and CPX-CEC-..-V3, CPX-E-CEC

1.20
03/08/2020
Inbetriebnahme IoT Gateway mit einem CPX Terminal CPX-IOT

This application nodes describes step by step how you

configure the CPX-IoT gateway with a CPX terminal

1.10
06/12/2019
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

3.10
02/07/2025
Show 15 more results ...
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.