Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description
BionicCellFactory
BionicCobot Sensitive helper for human-robot collaboration

Free-moving, intuitive to operate and predestined for direct human-robot collaboration; the pneumatic lightweight robot BionicCobot.

BionicFinWave Underwater robot with unique fin drive

The marine planarian, cuttlefish and Nile perch have one thing in common: in order to propel themselves, they use their fins to generate a continuous wave, which advances along their entire length. With this so-called undulating fin movement, the BionicFinWave also manoeuvres through a pipe system made of acrylic glass. At the same time the autonomous underwater robot is able to communicate with the outside world wirelessly and transmit data – such as the recorded sensor values for temperature and pressure – to a tablet.

BionicFlyingFox Ultra-lightweight flying object with intelligent kinematics

Flying fox as inspiration: thanks to its intelligent kinematics, the BionicFlyingFox is as agile and manoeuvrable in flight as its natural role model.

BionicKangaroo – energy-efficient jump kinematics based on a natural model Recovering, storing and releasing energy based on a natural model

With the BionicKangaroo, Festo has technologically reproduced the unique way a kangaroo moves. Like its natural model, it can recover the energy when jumping, store it and efficiently use it for the next jump.

BionicMobileAssistant Mobile robot system with pneumatic gripping hand

The BionicMobileAssistant moves autonomously in space and can independently recognise objects, grasp them adaptively and work on them together with humans. The processing of the acquired information is performed by a neural network that has been trained in advance using data augmentation.

BionicMotionRobot Lightweight robot with natural movement patterns

Sensitive and gentle or powerful and dynamic – the BionicMotionRobot’s movements are inspired by an elephant’s trunk and an octopus’s tentacles. The pneumatic lightweight robot features 12 degrees of freedom and, with a payload of three kilograms, can carry approximately its own weight.

BionicOpter Inspired by dragonfly flight

With the BionicOpter, Festo has technically mastered the highly complex flight characteristics of the dragonfly. Just like its model in nature, this ultralight flying object can fly in all directions, hover in mid-air and glide without beating its wings.

BionicSoftArm Modular pneumatic lightweight robot

Whether free and flexible movements or defined sequences, thanks to its modular design, the pneumatic lightweight robot can be used for numerous applications. In combination with various adaptive grippers, it can pick up and handle a wide variety of objects and shapes. At the same time, it is completely compliant and poses no danger to the user even in the event of a collision.

BionicSoftHand Pneumatic robot hand with artificial intelligence

Whether grasping, holding or turning, touching, typing or pressing – in everyday life, we use our hands as a matter of course for the most diverse tasks. The human hand is a true miracle tool of nature. What could be more logical than equipping robots in collaborative working spaces with a gripper that is modelled on this natural model and can learn through artificial intelligence to solve a wide variety of gripping and turning tasks?

BionicSwift Safe aerial acrobatics as a swarm

They are agile, nimble and can even fly loops and tight turns: the BionicSwifts. The five artificial swallows can move in a coordinated and autonomous manner in a defined airspace by interacting with a radio-based indoor GPS.

BionicTripod with FinGripper Flexible tripod with adaptive gripper - Energy-efficient movement and form-fit gripping
BionicWheelBot Walk and roll like a flic-flac spider

Inspired by the flic-flac spider, its natural role model, the BionicWheelBot can both walk and roll.

BionicWorkplace Human-robot collaboration with artificial intelligence

A pneumatic robot arm, artificial intelligence and intuitive operating concepts enable safe and efficient human–robot collaboration for production in batch size 1.

BioTech Automation Automation for biological transformation
Code of Conduct for Business Partners Guideline for suppliers

Within the Corporate Principles and the Festo Code of Conduct, the Festo Group and its employees have committed

themselves to support and apply the basic principles in the areas of human rights and working conditions, quality

and environmental management, health and safety as well as the fight against corruption and bribery.

CogniGame Control by the power of thought

New operational concepts for human-machine interaction

GogniGame is a reinterpretation of a table tennis simulation game,

which was launched on the market in the 1970s. As in table tennis, the players used a joystick in order to move a bar up and down the screen to hit a ball back to their opponent. If a player did not

manage to hit the ball, his opponent was awarded a point.

Cost-efficient production in the wood-working and wood processing industry
CyberKite Autonomous kite
Declaration of ingredients FN 940106 - Ban on / declaration of ingredients

Festo standard 940106 defines specifications for banned ingredients used in materials, as well as ingredients which are subject to mandatory declaration.

D-EE2201_01
D-FA1901 core product range – simply part of the solution
D-FC2001 SupraMotion 2020
D-LT2103 Media separated valves: handling of liquids and gases
D-LT2301 Parallel: Dispensing of liquids and storage of single small parts
D-PA2202 Improved reliability and productivity: Festo Motion Terminal in process automation
D-PD2101 Precise motion: wave audience on the high plateau
D-TA2001 Fast and precise movement creates melodies in Angklung
DualWingGenerator – power generation with the wing-beating principle Self-optimising system for ultimate plant efficiency and process reliability

With the DualWingGenerator, Festo has developed an extraordinary technology platform as part of the Bionic Learning Network. In contrast to conventional small wind power stations, the system uses two pairs of opposing wings instead of rotor blades to generate power.

D-WT2001 Reliable and Fast: Nereda® Technology
Show 30 more results ...