|
|
Product Overview for Process Automation
|
CatalogueFile and language versions
|
|
|
D-EE2201_01
|
BrochureFile and language versions
|
|
|
D-FC2001 SupraMotion 2020
|
BrochureFile and language versions
|
|
|
D-LT2103 Media separated valves: handling of liquids and gases
|
BrochureFile and language versions
|
|
|
D-LT2301 Parallel: Dispensing of liquids and storage of single small parts
|
BrochureFile and language versions
|
|
|
D-PA2202 Improved reliability and productivity: Festo Motion Terminal in process automation
|
BrochureFile and language versions
|
|
|
D-PD2101 Precise motion: wave audience on the high plateau
|
BrochureFile and language versions
|
|
|
D-TA2001 Fast and precise movement creates melodies in Angklung
|
BrochureFile and language versions
|
|
|
D-WT2001 Reliable and Fast: Nereda® Technology
|
BrochureFile and language versions
|
|
|
EnEffAH - Energy efficiency in production in the drive and handling technology field
Basic principles and measures
EnEffAH
stands for “ Energy Efficiency in Production in the Drive and Handling Technology Field” and is a joint project as part of the German
Government’s energy research programme.
...The goal of the project is to develop methods, tools and products to guarantee energy-efficient automation.
The correct selection of technology (effectiveness), and the correct operation (efficiency) are critical for energy efficiency and functionality. Based on an overall study, the project investigated both pneumatic and electric drive technology, including the functional chain and the use of these technologies in the field of handling and robotics.
|
BrochureFile and language versions
|
|
|
A Practical Energy Efficiency Solution for Life Science Utilizing Industry 4.0
“Internet of Things” (IoT) and “Industry 4.0” (I4.0) are buzzwords in the process manufacturing and automation world, with far-reaching benefits understood by most at a high level. But, what relevant and practical data and understanding can I4.0 bring your company in everyday operations, such as monitoring compressed air consumption, process optimization, enabling energy efficiencies, and providing preventative diagnostics?
|
Special publicationFile and language versions
|
|
|
Artificial hinged-wing bird with active torsion and partially linear kinematics
SmartBird
An artificial bird is introduced which was developed using two new
features in biologically-inspired flight, active torsion and partially linear
kinematics. Active torsion rests on well established theoretical
predictions in unsteady aerodynamics. The concept of partially linear
kinematics is inspired by zoological observations on flying locusts.
When the wings flap upwards, the servomotor for the active torsion
turns the outer wing from a positive angle of incidence within
a short fraction of the flapping period into a negative angle of incidence.
Between the turning points the angle of torsion remains
constant. Numerical calculations confirm the expected benefits
compared to passive torsion.
|
Special publicationFile and language versions
|
|
|
Dexterous Manipulation Using Hierarchical Reinforcement Learning
LearningGripper
On a novel pneumatic four-finger gripper with three degrees of freedom per finger we apply reinforcement learning to learn dexter- ous manipulation of objects. In order to reduce the search space, we implemented hierarchical learning on two levels. Low-level learning is used for basic movement primitives like grabbing, lifting or rotation of an object around three cartesian axes, whereas in high-level learning we use the already learned low-level actions to find a policy that ena- bles the gripper to move a target point on the surface of a sphere to the top position in a few seconds. It turns out that Q-learning with a finite state- and action space solves the learning task very well.
|
Special publicationFile and language versions
|
|
|
Installation, Commissioning & Maintenance services
|
Special publicationFile and language versions
|
|
|
Inventing a Micro Aerial Vehicle inspired by the mechanics of dragonfly flight
BionicOpter
Dragonfly flight is unique: Dragonflies can manoeuvre in all directions, glide without having to beat their wings and hover in the air. Their ability to move each of their four wings independently ena- bles them to slow down and turn abruptly, to accelerate swiftly and even to fly backwards. We looked into the mechanics of the dragonfly flight and managed to transfer its flight dynamics into an ultralight flying object: the Bionicüpter. With a wingspan of 63 cm and a body length of 44 cm, the model dragonfly weighs just 175 g. A brushless motor actuates the four wings and is used to alter the flapping fre- quency. Eight servo motors allow the amplitude and the twisting angle of each wing to be changed independently making the Bionicüpter almost as agile and fast as its natural role model. Here we present
how dragonfly flight dynamics can inspire future design of MAVs.
|
Special publicationFile and language versions
|
|
|
Spare parts catalogue
Spare parts finder for configured products like valve terminals and service units
|
Special publicationFile and language versions
|
|
|
The SLS-generated Soft Robotic Hand
An Integrated Approach using Additive Manufacturing and Reinforcement Learning
To develop a robotic system for a complex task is a time- consuming process. Merging methods available today, a new ap- proach for a faster realization of a multi-finger soft robotic hand is presented here. This paper introduces a robotic hand with four fingers and 12 Degrees of Freedom (DoFs) using bellow actuators. The hand is generated via Selective Laser Sintering (SLS), an Additive Manufacturing method. The complex task execution of a specific action, i.e. the lifting, rotating and precise positioning of a handling- object with this robotic hand, is used to structure the whole develop- ment process. To validate reliable functionality of the hand from the beginning, each development stage is SLS-generated and the targeted task execution is trained via Reinforcement Learning, a machine learning approach. Optimization points are subsequently derived and fed back into the hardware development. With this Concurrent Engineering strategy a fast development of this robotic hand is possible. The paper outlines the relevant key strategies and gives insight into the design process. At the end, the final hand with its capabilities is presented and discussed.
|
Special publicationFile and language versions
|
|
|
White Paper
New Air Services reduce the operational costs of pneumatic systems
|
Special publicationFile and language versions
|
|
|
White Paper: Bearing Technology
Key considerations for designers looking at bearing systems with linear axes
This White Paper contains information on:
- Use of electro mechanical axes with slides
- Possibilities of different slide bearings with single or double rail (giuding)
- Influences on lifetime, different guiding alternatives and design features
|
Special publicationFile and language versions
|
|
|
White Paper: Cleaning is a Must!
Cleaning is an absolute must if foodstuffs are to be produced hygienically. The highest priority here is afforded to avoiding the spread of germs and eliminating foreign particles. Proper cleaning reduces the downtime of your plant and systems, while protecting the consumer and your brand.
|
Special publicationFile and language versions
|
|
|
White paper: Plants based on the Lego principle
Modular automation with valve terminals
Smaller batches and different types of product in the same plant – these are the market demands to which more and more manufacturers in
the process industries need to adjust. The answer is plants based on the “Lego principle”. Users can add modules or switch them off in line
with requirements. But this is only possible with modular automation.
|
Special publicationFile and language versions
|
|
|
Multi-Carrier-System MCS® | Brochure
Brochure
|
External linkFile and language versions
|
|
|
Bistable valves in safety-related applications. An example.
Technical report TR-300003
Summary: Due to their bistable characteristics, bistable valves in certain applications present the user with tasks that seem to be difficult to solve. This application example is to show how a solution can be developed systematically taking the various operating states and operating transitions into account. Considering the various hazards in the various operating statuses of the machine appears a sensible approach to finding the solution. They require chronologically successive, different reactions of the safety circuit to implement the required protective measures.
|
BookFile and language versions
|
|
|
Festo AG & Co. KG bistable valves for safety-related applications
Technical Report - TR-300004
Summary: Technical Reports 2 and 3 [1-2] and DGUV Information FB HM-076 [3] already explained the circumstances under which bistable valves can be used in safety-related applications. The present report links these reports to the current product portfolio of Festo AG & Co. KG. The suitability of the bistable valves listed for safety-related applications can be confirmed taking the previous series of technical reports and respective technical documentation of the individual components into consideration.
|
BookFile and language versions
|