Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
Modulo Axis in Softmotion CMMP-AS-...M3/M0

How to use unlimited rotary axis in Softmotion V3.5

1.20
23/11/2016
MSE6-E2M with Omron PLC through EtherNet/IP MSE6-E2M with Omron PLC through EtherNet/IP; Library is included

This application note explains how to integrate the Festo MSE6-E2M-5000-FB36 with Omron Sysmac PLCs through EtherNet/IP network using the Sysmac Studio programming environment. The user will be able to control, parameterize & diagnose the error details of the Festo MSE6-E2M.

1.10
09/02/2026
MSE6-E2M-5000-FB36-AGD commissioning with ROCKWELL STUDIO5000 in ETHERNET/IP Network MSE6; ROCKWELL STUDIO5000; Library included

This Application Note helps to integrate Allen-Bradly PLC with MSE6-E2M Energy Efficient Module through EtherNet-IP Net-work. Also Provide Detailed Description About Hardware & Soft-ware Configuration.

1.20
23/07/2021
PCS7 V10 Compatibility PCS7 V10 Compatibility

This application note guides the user to migrate and resolve errors in PCS7 V10.1 SP1 where CTEU_PCS7 and CPX_PCS7 libraries are installed.

1.10
19/01/2026
Power supply concept CPX with OVEM CPX; OVEM; Duo-cable

System integration with regard to the power supply concept for the CPX interlinking block and the OVEM are illustrated by sev-eral examples in this document.

1.10
09/05/2017
Programming CPX-F8DE-P and the CPX-FVDA-P2 in TIA Portal V14 SP1 CPX-F8DE-P; CPX-FVDA-P2; TIA V14; Example project included

The application note contains an explanation how to program CPX-F8DE-P bit oriented and the CPX-FVDA-P2 in TIA Portal V14 SP1 V14 SP1 and example program

1.30
23/07/2021
Programming CPX-F8DE-P in TIA Portal CPX-FB34; CPX-F8DE-P

The application node contains an explanation how to program CPX-F8DI-P in TIA Portal in different safety applications

V1.10
01/08/2016
QuickStart CPX-FB37 EtherCAT on TwinCAT 3 CPX-FB37; TwinCAT3; Example project included

Setting up a CPX-FB37 EtherCAT slave module on Beckhoff TwinCAT 3.

1.10
03/03/2021
Replacing an old CPX-FB36 EtherNet/IP Bus Node Replacing an old CPX-FB36 EtherNet/IP Bus Node

This document has information combined from multiple resources for the intention of reducing the effort of a user who is configuring this application type

1.10
26/02/2024
Replacing an old CPX-FB37 EtherCAT Bus Node Replacing an old CPX-FB37 EtherCAT Bus Node

This document has information combined from multiple resources for the intention of reducing the effort of a user who is configuring this application type.

1.10
26/02/2024
Security white paper for Festo controllers

This document is intended to provide users of Festo control products with an introduction and support on how Festo controllers can be used as securely as possible from the point of view of cyber security.

V03
25/05/2023
Siemens IOL_CALL with CPX I-Port Master for IO Link Devices CPX-CTEL-2-M12-5POL-LK; SDAT-MHS-M80-1L-SA-E-0.3-M8

 Over the Siemens IOL_CALL block The parameters can be modified by an IO Link device / read acyclic. Because on our CPX CTEL 2 M12-5POL-LK not a IODD can be included, is a parame-terization of eg a Festo IO Link device (SDAT MO Link device (SDAT MHS M80-1L-SA-E-0.3-M8) only via this function module is possible

1.10
24/02/2015
Siemens TIA Portal with CPX I-Port Master for IO Link Devices CPX-CTEL-2-M12-5POL-LK; SDAT-MHS-M80-1L-SA-E-0.3-M8; CPX-FB34; IM151-8F PN/DP CPU

Basic steps for commissioning the CPX-CTEL-2-M12-5POL-LK with our SDAT-MHS-M80-1L-SA-E-0.3-M8 in the TIA Portal are described in this application note

1.10
09/06/2016
Special SoftMotion settings/Homing issues for CPX-CEC-M1-V3 CPX-CEC-C1/M1-V3

The document describes special CODESYS V3 settings for CPX-CEC-M1-V3 (SoftMotion) controllers and the use of Soft- Motion homing function "MC_Home" in combination with Festo drives.

1.20
23/06/2016
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.