Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
FSA-202304 - Security Advisory - MSE6-C2M/D2M/E2M Incomplete User Documentation of Remote Accessible Functions

Incomplete user documentation of undocumented, authenticated test mode and further remote accessible functions. The supported features may be covered only partly by the corresponding user documentation.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.0.0
Festo CPX and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects CPX-FB36 and E2M via EtherNet/IP with Rockwell Factory Talk Edge Gateway and Smart Objects

How to extract data from CPX-FB36 systems using the built-in auto-discovery feature of Factory Talk Edge Gateway by Rockwell Automation.  What are the use cases of this data, and how to supplement it by using Factory Talk Smart Objects.

1.10
06/12/2022
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.4
12/10/2026
MSE6 C2M CPX FB36 with LS PLC through Modbus TCP MSE6 C2M CPX FB36 with LS PLC through Modbus TCP; Library included

This application note describes the Auto Control Function block which is used for controlling the functionality of Festo MSE6- C2M-5000-FB36

1.10
02/01/2025
MSE6-C2M 5000 FB36 commissioning in EtherNet/IP network Rockwell Logix PLC MSE6-C2M FB36 Commissioning Eth/IP; Library included

his Application Note will help to integrate Allen-Bradly Logix PLC with MSE6-C2M Energy Efficient Module through EtherNet-IP Network. Also provide detailed description about Hardware & Software configuration.

1.20
05/04/2024
MSE6-C2M Commissioning with Keyence KV-8000 PLC by EtherNet/IP Network MSE6-C2M; Keyence KV-8000 PLC; EtherNet/IP Network; Library included

This Application Note helps the user to integrate MSE6-C2M 5000-FB36 modules with Keyence KV-8000 PLC through EtherNet/IP network. Also describes about which are the steps that need to be taken in order to integrate library for MSE6-C2M into a Keyence KV STUDIO programming environment. And it also explains a new Auto Mode library.  

1.20
14/08/2024
MSE6-C2M CPX FB36 with Festo PLC through Modbus TCP library MSE6-C2M CPX FB36 with Festo PLC through Modbus TCP library; Library included

This application note provides a step-by-step guide on integrating MSE6-C2M-5000-FB36 modules with Festo PLC using the Modbus TCP protocol, and incorporating the MSE6-C2M library into the Codesys development environment.

1.10
04/02/2025
MSE6-C2M Integration with Beckhoff TwinCAT 3 PLC through EtherCAT Network MSE6-C2M, with Beckhoff TwinCAT 3 PLC through EtherCAT Network Library included

This application note will describe how to integrate MSE6-C2M
energy efficient module from Festo with Beckhoff Twin-CAT 3 PLC
through EtherCAT network. Also describes which are the steps that
need to be taken, in order to integrate library for MSE6-C2M into a
Beckhoff TwinCAT 3 programming environment.

1.10
18/05/2022
MSE6-C2M Integration with Emerson DeltaV using EtherNet/IP MSE6-C2M Integration with Emerson DeltaV using EtherNet/IP; Library included

This application note gives detailed explanation of integration procedure and library for Festo MSE6-C2M-5000-FB36 with Emerson DeltaV through EtherNet/IP.

1.10
21/08/2024
MSE6-C2M Integration with Festo PLC through EtherCAT Network MSE6-C2M Integration with Festo PLC through EtherCAT Network Library included

This application note will describe how to integrate MSE6-C2M energy
efficient module from Festo with Festo PLC through EtherCAT network.
Also describes which are the steps that need to be taken in order to
integrate library for MSE6-C2M into a Festo CodeSys programming
environment.

1.20
16/05/2025
MSE6-C2M Integration with Mitsubishi-PLC (GxWorks3) by EtherNetIP Network MSE6-C2M; Mitsubishi FX5U/ R-Series PLC (GxWorks3) by ETH/IP; Library included

This application note will describe how to integrate MSE6-C2M Energy Efficient Module from Festo with Mitsubishi FX5U and R-Series PLC through EtherNet/IP network. Also describes which are the steps that need to be taken in order to integrate library for MSE6-C2M into a Mitsubishi GxWorks3 programming environment.

1.10
04/07/2023
MSE6-C2M with Mitsubishi IQ-R PLC through Modbus TCP Library MSE6-C2M with Mitsubishi IQ-R PLC through Modbus TCP Library; Library is included

This Application Note gives a step by step description of how to integrate Festo MSE6-C2M-5000-FB36 modules with Mitsubishi iQ-R PLC through Modbus TCP network using Simple CPU Communication in GX Works3 programming environment.

1.10
22/10/2025
MSE6-C2M_Omron_Integration through EtherCAT MSE6-C2M_Omron_Integration through EtherCAT; Library and sample program included

This Application Note will help to integrate MSE6-C2M Energy Efficient Module with Omron PLC through EtherCAT Network. Also provide detailed description about Hardware & Software Configuration. In addition it include an Auto Control Function Block. 

1.10
08/08/2024
MSE6-C2M-5000-FB33/FB34/FB35 integration with S7-1500 PLC using TIA Portal MSE6-C2M-5000-FB33/FB34/FB35; Siemens TIA Portal; Library included

This Application Note helps the user to integrate MSE6-C2M- 5000-FB33/34/35 modules with Siemens S7-1500 PLC using TIA Portal 15.1. Also this application note briefly describes the Function Blocks which are used for controlling the functionality of MSE6-C2M-5000-FB33/FB34/FB35

1.10
15/01/2020
MSE6-C2M-5000-FB36 with LS Electric PLC through Eth/IP MSE6-C2M-5000-FB36 with LS Electric PLC through Eth/IP; Library included

This document describe the steps to integrate MSE6-C2M-5000-FB36 modules with LS Electric PLC using EtherNet/IP and to incorporate the MSE6-C2M library into the LS Electric XG5000 programming environment.

It also include the Auto Control Function block which is used for controlling the functionality of Festo MSE6- C2M-5000-FB36

1.10
17/03/2025
MSE6-C2M-5000-FB43_FB44_FB45 integration with S7-1500 PLC using TIA Portal MSE6-C2M-5000-FB43_FB44_FB45; S7-1500 PLC; Library included

This Application Note helps the user to integrate MSE6-C2M 5000-FB43/44/45 modules with Siemens S7-1500 PLC using TIA Portal 15.1. Also this application note briefly describes the Function Blocks which are used for controlling the functionality of MSE6-C2M-5000-FB43/FB44/FB45. In addition it includes a description of the Auto Control Function.

1.10
15/02/2024
MSE6-E2M Function Blocks for CODESYS V3 MSE6-E2M, EtherCAT, Modbus/TCP

This application note will describe which are the steps that need to be taken in order to integrate the Function Blocks for MSE6- E2M with Modbus/TCP or EtherCAT into a CODESYS V3 pro-gramming environment.

1.10
24/05/2019
MSE6-E2M-5000-FB13 Profibus integration with Siemens PLC using TIA Portal 15 MSE6; TIA

This Application Note helps the user to integrate MSE6-E2M- 5000-FB13 module with Siemens PLC using TIA Portal 15. Also this application note briefly describes the Function Blocks which are used for controlling the functionality of MSE6-E2M-5000 module.

1.10
24/05/2019
MSE6-E2M-5000-FB33 integration with S7-1500 PLC using TIA Portal 15 MSE6; Siemens TIA 15; Festo FB33

This Application Note helps the user to integrate MSE6-E2M- 5000-FB33 module with Siemens S7-1500 PLC using TIA Portal 15. Also this application note briefly describes the Function Blocks which are used for controlling the functionality of MSE6- E2M-5000 module.

1.10
24/05/2019
MSE6-E2M-5000-FB36-AGD commissioning with ROCKWELL STUDIO5000 in ETHERNET/IP Network MSE6; ROCKWELL STUDIO5000; Library included

This Application Note helps to integrate Allen-Bradly PLC with MSE6-E2M Energy Efficient Module through EtherNet-IP Net-work. Also Provide Detailed Description About Hardware & Soft-ware Configuration.

1.20
23/07/2021
MSE6-E2M-5000-FB44 integration with S7-1500 PLC using TIA Portal 15 MSE6-E2M-5000-FB44 Siemens S7-1500 PLC TIA Portal 15; Library included

This Application Note helps the user to integrate MSE6-E2M 5000-FB44 module with Siemens S7-1500 PLC using TIA Portal 15. Also this application note briefly describes the Function Blocks which are used for controlling the functionality of MSE6- E2M-5000 module.

1.10
16/05/2023
MSE6-E2M-FB37-Commissioning with TwinCat 3 and Beckhoff PLCMSE6-E2M-FB37-Commissioning with TwinCat 3 and Beckhoff PLC MSE6-E2M-FB37; TwinCat 3; Beckhoff PLC, Library included

This Application Note will helps to integrate Beckhoff PLC with MSE6-E2M Energy Efficient Module through EtherCAT Network. Also Provide Detailed Description About Hardware & Software Configuration.

1.10
28/04/2023
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.