What is green hydrogen?

Hydrogen is produced via electrolysis – a process in which water is split into hydrogen and oxygen using electricity. An important factor for producing green hydrogen is that the electricity used must come from renewable sources.

This is in contrast to, for example:

  • Grey hydrogen produced from fossil fuels
  • Pink hydrogen, which does not produce CO₂ as it uses nuclear energy, but does produce radioactive waste
  • And blue hydrogen, in which CO₂ is separated and stored (carbon capture)

That means electrolysis is the first – and crucial – step in the hydrogen value chain.

Discover how automation can improve processes along the entire value chain.

1. Production

The starting point in the hydrogen value chain is electrolysis. Water is split into hydrogen and oxygen using electricity from renewable energy sources. Different electrolyser technologies are used depending on the framework conditions:

  • PEM for flexible load change,
  • Alkaline processes based on proven processes, or
  • SOEC for maximum efficiency through high-temperature electrolysis

An automated controller ensures that the temperature, pressure and media flows are always within the optimum range, creating maximum efficiency and plant and system availability.

2. Hydrogen treatment

Freshly produced hydrogen is rarely pure right from the start. It often contains moisture, oxygen residues or other contaminants. Special systems for hydrogen treatment bring it to the required quality – a purity of up to 99.999%. This is crucial in order to prevent corrosion, loss of efficiency or damage to downstream systems. Automated systems monitor all relevant process parameters in real time, react to deviations and optimise the use of energy and equipment. This not only increases safety, but also makes the entire process more efficient and easier to scale.

3. Compression and storage

Hydrogen has a very low energy density at standard pressure. There are several ways to transport or store it efficiently:

  • Gaseous compression with compressors at 350 to 500 bar
  • Liquefaction by cooling it to very low temperatures, or
  • The chemical conversion of a molecule into hydrogen-containing compounds

Pressure control, filling and monitoring must be seamless and reliable. Precise valve technology and reliable sensors ensure safe, stable operation.

4. Distribution and transport

The route from the place of production to the place of use can look very different and includes pipelines, trailers to on-site production. Whatever the method, transport must be safe, low-loss and economical. Automated monitoring systems detect leakages or pressure fluctuations at an early stage and control the flow rate and valve positions in real time.

5. Application

Green hydrogen has a wide range of applications. It can be used directly as a molecule in the chemical industry and for steel production and is also used in the production of synthetic natural gas or fuels. In fuel cells, hydrogen can then be used again to generate electricity, contributing to low-carbon mobility by reducing CO2 emitted by vehicles. Every application brings its own challenges, but automation technology helps to master them flexibly and reliably. Processes can be adapted to changing conditions and load profiles at any time and meet important safety requirements.

10 Common Mistakes to Avoid in Hydrogen Automation ​

Hydrogen automation is complex, and mistakes can be costly. This checklist helps you prevent risks and design safer, scalable systems. You’ll learn how to: ​

  • Avoid the 10 most common errors ​
  • Save time and reduce rework ​
  • Strengthen safety and compliance
Get your free Checklist today

Why automation is key to scaling

Green hydrogen is only competitive if it can be produced and utilised safely, reliably and efficiently. This can be achieved when using automation solutions with valve terminals and modular controllers in combination with real-time diagnostic functions. For example, they can help to:

  • Minimise downtimes
  • Meet regulatory requirements (ATEX, SIL)
  • Reduce system complexity

Festo – your partner along the entire value chain

Festo supports companies along the entire hydrogen value chain with industry-specific automation solutions. With our scalable systems, digital diagnostic functions and certified components, we help to make processes safe and future-proof, whether in electrolysis, gas treatment or mobile applications such as trailer control systems.

The green hydrogen value chain is more than just a topic for the future

It is already a reality right now and its importance will continue to grow. Those who understand the entire chain can make well-informed decisions and integrate suitable solutions at an early stage.

Would you like to know more?

Efficient hydrogen control with Festo – from start to finish

Are you already working on a specific application?

Talk to our experts about your automation solution