This technology plays a crucial role in the operation of automated machines and systems across various applications. Its primary function is to precisely control motor movement, making it a key component in operations where high performance and reliability are critical.

But how exactly does it work, and what are its main components? Let’s explore the structure, operation, types, and benefits of servo drives in industrial automation.

What is a servo drive?

A servo drive is a motion control system that regulates a motor's position, speed, and torque in real time. Widely used in industrial automation, it enables high-efficiency, repeatable, and precise movements.

The term "servo” refers to the system's ability to automatically adjust operating parameters based on feedback. This means the motor's operation is continuously fine-tuned by correcting any deviations, ensuring that the desired motion is achieved accurately.

Key Components

A servo drive system consists of three core elements that work together to ensure precise motion control:

  • Servo motor – Converts electrical energy into mechanical motion.
  • Controller – Processes command signals and manages motor operation.
  • Encoder – Monitors motor behavior and sends real-time data (position, speed, torque) back to the controller.

These components form a closed-loop system, enabling dynamic adjustments and precise control through continuous feedback.

Operating principle of a servo drive

The system operates through real-time interaction among its three main components. This closed-loop process enables continuous corrections to achieve precise motion control.

Control signal

The controller generates a control signal based on digital commands that define the motor's movement—its position, speed, and applied torque. These commands are interpreted and converted into electrical signals that are sent to the motor.

Motion execution

The motor receives the signal and converts electrical energy into mechanical motion, either linear or rotary, depending on its design. The system dynamically adjusts speed and torque based on the specific requirements of the application.

Feedback and correction

The encoder continuously monitors the motor's position, speed, and output torque. This information is sent to the controller, which compares the real-time values with the desired ones and makes the necessary corrections to maintain precise control.
This constant feedback loop ensures stable and accurate performance—even under variable load or environmental conditions.

Types of servo motors in industrial automation

Different types of servo motors are used depending on the specific requirements of the application. The most common types in industrial environments include:

DC servo motors

Powered by direct current, these motors provide excellent control of speed and torque at low RPMs. Their fast response and affordability make them ideal for low to mid-complexity automation systems.

AC servo motors

These motors use alternating current and are well-suited for applications requiring higher power and a broad range of speeds. Their robust construction ensures reliable performance in demanding industrial environments.

Stepper motors

Used for position control, these motors divide movement into small steps. They are ideal for applications such as CNC machines, 3D printers, and cost-effective positioning systems.

Advantages of using servo drives in industry

These systems offer multiple benefits that make them essential components across various industrial sectors. For high-performance and integrated motion control, systems like Festo’s servo drives and motors CMMT-AS/CMMT-ST and EMMT-AS provide advanced solutions. Key advantages include:

High precision and repeatability

A standout feature is the ability to execute precise, repeatable movements. Continuous sensor feedback enables real-time adjustments for consistent and accurate results.

Energy efficiency

Servo drives adjust the energy used based on the exact demands of the motion, unlike conventional motors that run at full power. This translates into significant energy savings—especially in variable-speed or variable-torque processes.

Flexibility and adaptability

Servo systems can be configured to meet the specific needs of virtually any application—from small devices to large-scale industrial systems. Their versatility makes them ideal for sectors such as automotive, pharmaceuticals, and electronics.

How does a servo motor work?

The servo motor is the component that transforms electrical signals into mechanical motion.

Upon receiving a signal from the controller, the motor (DC, AC, or stepper) produces rotational or linear movement. Designed for high-precision operation, it adjusts rotation and torque based on application requirements.

Real-time feedback from the position sensor enables the system to detect and correct deviations instantly, ensuring precise and consistent performance.

How does a servo motor encoder work?

The encoder measures the position of the motor shaft and sends this data to the controller.

There are various types of encoders—such as optical and magnetic—differing in precision and cost. Regardless of type, they all play a critical role in the feedback loop, enabling real-time adjustments and precise motor control.

Connect with industrial motion control experts

Servo drives are a cornerstone of modern automation due to their ability to deliver precision, energy efficiency, and adaptability across a wide range of production processes.

By integrating a motor, controller, and encoder into a synchronized system, they execute complex movements with high accuracy and repeatability.

Looking to boost the performance of your automation systems?
Connect with Festo and explore our advanced motion control solutions powered by servo technology.