|
|
Bionic Tripod 3.0
A highly dynamic flexible tripod
A highly dynamic flexible tripod
|
BrochureFile and language versions
|
|
|
BionicANTs – cooperative behaviour based on a natural model
Highly integrated individual systems to solve a common task
For the BionicANTs, Festo has not only taken the delicate anatomy of the natural ant as a role model. For the first time, the cooperative behaviour of the creatures is also transferred to the world of technology using complex control algorithms.
|
BrochureFile and language versions
|
|
|
BionicCellFactory
|
BrochureFile and language versions
|
|
|
BionicCobot
Sensitive helper for human-robot collaboration
Free-moving, intuitive to operate and predestined for direct human-robot collaboration; the pneumatic lightweight robot BionicCobot.
|
BrochureFile and language versions
|
|
|
BionicFinWave
Underwater robot with unique fin drive
The marine planarian, cuttlefish and Nile perch have one thing in common: in order to propel themselves, they use their fins to generate a continuous wave, which advances along their entire length. With this so-called undulating fin movement, the BionicFinWave also manoeuvres through a pipe system made of acrylic glass. At the same time the autonomous underwater robot is able to communicate with the outside world wirelessly and transmit data – such as the recorded sensor values for temperature and pressure – to a tablet.
|
BrochureFile and language versions
|
|
|
BionicFlyingFox
Ultra-lightweight flying object with intelligent kinematics
Flying fox as inspiration: thanks to its intelligent kinematics, the BionicFlyingFox is as agile and manoeuvrable in flight as its natural role model.
|
BrochureFile and language versions
|
|
|
BionicKangaroo – energy-efficient jump kinematics based on a natural model
Recovering, storing and releasing energy based on a natural model
With the BionicKangaroo, Festo has technologically reproduced the unique way a kangaroo moves. Like its natural model, it can recover the energy when jumping, store it and efficiently use it for the next jump.
|
BrochureFile and language versions
|
|
|
BionicMobileAssistant
Mobile robot system with pneumatic gripping hand
The BionicMobileAssistant moves autonomously in space and can independently recognise objects, grasp them adaptively and work on them together with humans. The processing of the acquired information is performed by a neural network that has been trained in advance using data augmentation.
|
BrochureFile and language versions
|
|
|
BionicMotionRobot
Lightweight robot with natural movement patterns
Sensitive and gentle or powerful and dynamic – the BionicMotionRobot’s movements are inspired by an elephant’s trunk and an octopus’s tentacles. The pneumatic lightweight robot features 12 degrees of freedom and, with a payload of three kilograms, can carry approximately its own weight.
|
BrochureFile and language versions
|
|
|
BionicOpter
Inspired by dragonfly flight
With the BionicOpter, Festo has technically mastered the highly complex flight characteristics of the dragonfly. Just like its model in nature, this ultralight flying object can fly in all directions, hover in mid-air and glide without beating its wings.
|
BrochureFile and language versions
|
|
|
BionicSoftArm
Modular pneumatic lightweight robot
Whether free and flexible movements or defined sequences, thanks to its modular design, the pneumatic lightweight robot can be used for numerous applications. In combination with various adaptive grippers, it can pick up and handle a wide variety of objects and shapes. At the same time, it is completely compliant and poses no danger to the user even in the event of a collision.
|
BrochureFile and language versions
|
|
|
BionicSoftHand
Pneumatic robot hand with artificial intelligence
Whether grasping, holding or turning, touching, typing or pressing – in everyday life, we use our hands as a matter of course for the most diverse tasks. The human hand is a true miracle tool of nature. What could be more logical than equipping robots in collaborative working spaces with a gripper that is modelled on this natural model and can learn through artificial intelligence to solve a wide variety of gripping and turning tasks?
|
BrochureFile and language versions
|
|
|
BionicSwift
Safe aerial acrobatics as a swarm
They are agile, nimble and can even fly loops and tight turns: the BionicSwifts. The five artificial swallows can move in a coordinated and autonomous manner in a defined airspace by interacting with a radio-based indoor GPS.
|
BrochureFile and language versions
|
|
|
BionicTripod with FinGripper
Flexible tripod with adaptive gripper - Energy-efficient movement and form-fit gripping
|
BrochureFile and language versions
|
|
|
BionicWheelBot
Walk and roll like a flic-flac spider
Inspired by the flic-flac spider, its natural role model, the BionicWheelBot can both walk and roll.
|
BrochureFile and language versions
|
|
|
BionicWorkplace
Human-robot collaboration with artificial intelligence
A pneumatic robot arm, artificial intelligence and intuitive operating concepts enable safe and efficient human–robot collaboration for production in batch size 1.
|
BrochureFile and language versions
|
|
|
BioTech Automation
Automation for biological transformation
|
BrochureFile and language versions
|
|
|
Code of Conduct for Business Partners
Guideline for suppliers
Within the Corporate Principles and the Festo Code of Conduct, the Festo Group and its employees have committed
themselves to support and apply the basic principles in the areas of human rights and working conditions, quality
and environmental management, health and safety as well as the fight against corruption and bribery.
|
BrochureFile and language versions
|
|
|
CogniGame
Control by the power of thought
New operational concepts for human-machine interaction
GogniGame is a reinterpretation of a table tennis simulation game,
which was launched on the market in the 1970s. As in table tennis, the players used a joystick in order to move a bar up and down the screen to hit a ball back to their opponent. If a player did not
manage to hit the ball, his opponent was awarded a point.
|
BrochureFile and language versions
|
|
|
Cost-efficient production in the wood-working and wood processing industry
|
BrochureFile and language versions
|
|
|
CyberKite
Autonomous kite
|
BrochureFile and language versions
|
|
|
Declaration of ingredients
FN 940106 - Ban on / declaration of ingredients
Festo standard 940106 defines specifications for banned ingredients used in materials, as well as ingredients which are subject to mandatory declaration.
|
BrochureFile and language versions
|
|
|
D-EE2201_01
|
BrochureFile and language versions
|
|
|
D-FA1901 core product range – simply part of the solution
|
BrochureFile and language versions
|
|
|
D-FC2001 SupraMotion 2020
|
BrochureFile and language versions
|
|
|
D-LT2103 Media separated valves: handling of liquids and gases
|
BrochureFile and language versions
|
|
|
D-LT2301 Parallel: Dispensing of liquids and storage of single small parts
|
BrochureFile and language versions
|
|
|
D-PA2202 Improved reliability and productivity: Festo Motion Terminal in process automation
|
BrochureFile and language versions
|
|
|
D-PD2101 Precise motion: wave audience on the high plateau
|
BrochureFile and language versions
|
|
|
Drive productivity on the road
Get the most out of your assets.
In tire production, every second and every kilowatt counts. Discover how you can become faster and more efficient in all areas with solutions from Festo, including through clever retrofitting.
|
BrochureFile and language versions
|