|
|
D-TA2001 Fast and precise movement creates melodies in Angklung
|
BrochureFile and language versions
|
|
|
DualWingGenerator – power generation with the wing-beating principle
Self-optimising system for ultimate plant efficiency and process reliability
With the DualWingGenerator, Festo has developed an extraordinary technology platform as part of the Bionic Learning Network. In contrast to conventional small wind power stations, the system uses two pairs of opposing wings instead of rotor blades to generate power.
|
BrochureFile and language versions
|
|
|
D-WT2001 Reliable and Fast: Nereda® Technology
|
BrochureFile and language versions
|
|
|
eMotionButterflies – ultralight flying objects with collective behaviour
Coordinated flying thanks to indoor GPS
With the bionic butterflies, for the first time Festo combines the ultralight construction of artificial insects with collision-free flying behaviour in a collective. For coordination purposes, the eMotionButterflies make use of a guidance and monitoring system, which could be used in the networked factory of the future.
|
BrochureFile and language versions
|
|
|
eMotionSpheres – collision-free motion of autonomous systems in a space
Flying objects with bionic drive – individual and collective
With the eMotionSpheres, Festo shows how several flying objects can move in a coordinated manner and within a defined space. Whether individually or collectively – even in chaotic situations, there are no collisions as the balls move out of each other’s way.
|
BrochureFile and language versions
|
|
|
Energy efficiency@Festo
|
BrochureFile and language versions
|
|
|
ExoHand
Human-Machine cooperation
New scope for interaction between humans and machines
The ExoHand from Festo is an exoskeleton that can be worn like
a glove. The fingers can be actively moved and their strength amplified; the operator’s hand movements are registered and transmitted to the robotic hand in real time.
|
BrochureFile and language versions
|
|
|
Festo Multi Axis Solution
Control up to 4 axes from a single robot!
The Festo Multi Axis Solution amplifies the capabilities of the UR robot and simplifies integration by using off-the-shelf mechanical and electrical components readily available worldwide.
|
BrochureFile and language versions
|
|
|
Festo Sustainability Report 2020
|
BrochureFile and language versions
|
|
|
Fin Ray Effect®
The Fin Ray Effect® or bionics in factory automation
|
BrochureFile and language versions
|
|
|
FlexShapeGripper – gripping modelled on a chameleon’s tongue
Soft gripping for various tasks
Gripping modelled on a chameleon’s tongue: by inverting its elastic silicone cap, the FlexShapeGripper can pick up, gather and set back down the widest range of objects in one procedure – without the need for a manual conversion.
|
BrochureFile and language versions
|
|
|
Folder for tubing and fittings combinations
Well combined: tubing/fitting combinations for all applications!
Precise selection of the right tubing/fitting combination is above all dependent on the application. Applications often have a single feature that quickly defines the right selection. The overview of our most popular tubing/fitting combinations will help you to make the right choice quickly and reliably.
|
BrochureFile and language versions
|
|
|
Hovercraft Vector
Hovercraft with thrust vector control
|
BrochureFile and language versions
|
|
|
Humanoid Muscle-Robot
A robot using Fluidic Muscle as actuator!
|
BrochureFile and language versions
|
|
|
Insulated hot-air balloon
A hot-air balloon with fuel consumption reduced by half
|
BrochureFile and language versions
|
|
|
InteractiveWall
Real time interactive architecture
InteractiveWall transforms the behaviour of people standing in front of it into motion, light and music in real time and thus interacts with the user.
|
BrochureFile and language versions
|
|
|
LearningGripper
Gripping and positioning through independent learning
The LearningGripper from Festo looks like an abstract form of the human hand. The four fingers of the gripper are driven by twelve pneumatic bellows actuators with low-level pressurisation. Thanks to the machine learning process, the gripper is able to teach itself to carry out complex actions such as the targeted gripping and positioning of an object.
|
BrochureFile and language versions
|
|
|
MCS® - Multi Carrier System
Maximum flexibility in the machine
With the innovative Multi-Carrier-System MCS®, a joint development by Festo and Siemens, you are on the right track. Thanks to the modular design of the transport system, it can be combined with conventional transport solutions, adding the functionality of the MCS® where needed in the process.
|
BrochureFile and language versions
|
|
|
Modular Lightweight Handling
Handling from a construction kit
|
BrochureFile and language versions
|
|
|
Molecubes
A programmable robot system
Molecubes – learning by experimenting and programming
|
BrochureFile and language versions
|
|
|
MultiChoiceGripper – variable gripping based on the human hand
An adaptive and flexible gripper for the widest range of shapes
Just like its natural role model, the MultiChoiceGripper combines different grip types. Its fingers can therefore be switched over so that they can either grip in a parallel or centric direction – without requiring any conversion.
|
BrochureFile and language versions
|
|
|
Official Partner: our common route towards greater success
There are lots of good reasons to become a Festo
Official Partner. Find out the benefits of this
partnership for you and your customers!
|
BrochureFile and language versions
|
|
|
OptoFluidic
Real-time optical analysis
Real-time optical analysis of fluids
|
BrochureFile and language versions
|
|
|
Overview of one-way flow control valves
|
BrochureFile and language versions
|
|
|
Partner for technical skills development in the mining and metals industry
|
BrochureFile and language versions
|
|
|
performance
Company profile
Information about Festo in general
Facts and figures
|
BrochureFile and language versions
|
|
|
PhotoBionicCell
|
BrochureFile and language versions
|
|
|
Pictures of the Festo plants
This overview shows pictures of the headquarter, technology factory Scharnhausen and the plant in Rohrbach.
(zip file contains 3 documents with various pictures, one file for each plant)
|
BrochureFile and language versions
|
|
|
Pneumatic lightweight structures
Documentation of development
|
BrochureFile and language versions
|
|
|
PowerGripper
Grasping concept on the model of the bird
Research project for the development of new gripper systems
PowerGripper is a university project conducted as part of the Bionic Learning Network. Together with renowned educational
establishments, institutes and development companies, Festo is investigating the transfer of biological principles to technology in
order to generate innovative solutions for industry.
|
BrochureFile and language versions
|