Pressure dew point is the temperature to which compressed air can cool, at its actual working pressure, before the water vapour inside it starts to condense.
At that point, the air is saturated. If the temperature drops further, the excess moisture separates from the air as condensate.
A simple way to think about it:
For example, compressed air with a pressure dew point of 3 °C can cool down to 3 °C before condensation begins. If the air temperature drops below that, water can form in the system.
That makes pressure dew point a practical moisture limit for compressed air systems.
Want to learn more about compressed air preparation?
📘 Download our whitepaper: Answers to the 5 most frequently asked questions about air prep
Pneumatic components are designed to work with clean, prepared compressed air. Moisture is one form of compressed air contamination that can reduce component reliability and product quality.
Water in pipes or components can cause corrosion of internal surfaces and shorten service life. It can also wash away lubrication, increase friction and make moving parts less predictable.
The first signs are often subtle. A cylinder moves less smoothly. A valve responds more slowly. A pneumatic tool loses consistency. Over time, these small symptoms can turn into unplanned downtime, quality issues or premature component replacement.
In critical industries, the stakes are higher. In food, pharmaceuticals, electronics and medical technology, compressed air quality can influence product safety, hygiene, process stability and compliance.
Dry air protects more than only components. It also protects output.
The right pressure dew point depends on the conditions around the application, not just on the compressed air system itself.
Start by checking three factors:
These factors define how dry the compressed air needs to be. A standard pneumatic application in a controlled indoor environment will not have the same requirement as an outdoor installation or a sensitive production process.
As a practical rule, the pressure dew point should be at least 10 °C lower than the lowest expected ambient temperature around the system. In technical contexts, this temperature difference is often written as 10 K.
For example, if the lowest expected temperature near the application is 13 °C, the pressure dew point should be 3 °C or lower. This margin helps prevent condensate from forming when temperatures fluctuate.
For many standard pneumatic applications, a pressure dew point of around 3 °C is sufficient.
Applications in colder areas, outdoor installations, sensitive production environments or processes with strict air quality requirements may need much lower values such as -20 °C, -40 °C or -70 °C.
The goal is not always to achieve the lowest possible pressure dew point. The goal is to define a value that keeps the air dry enough for the application and stable enough for the operating environment.
Lowering pressure dew point means removing more water vapour from the compressed air before it reaches the application. The right method depends on how dry the air must be, where the risk appears in the system and how the compressed air network is designed.
Before choosing a dryer, check the basic compressed air preparation setup. The system should match the required air purity, flow rate, working pressure, ambient temperature range and distance between air preparation and point of use.
A dryer cannot compensate for every design issue. If the flow rate is too high, the dryer is undersized or the preparation unit sits too far from the critical application, moisture problems can still appear downstream.
Three dryer technologies are commonly used to lower pressure dew point:
For a detailed comparison of these technologies, read our guide to choosing the right compressed air dryer.
The location of the dryer can affect how reliably the target pressure dew point is maintained.
Central drying treats compressed air before it enters the wider network. This works well when the whole system needs the same air quality and the distribution network is well controlled.
Decentralised drying treats the air closer to the machine or point of use. This can be useful when only selected applications need drier air, or when long pipe runs, cold areas or local temperature changes increase condensation risk. Also, the impact on pressure drop, thus the effecienct of the system, can be optimized by implement decentral drying.
Many systems use both. Central drying provides the base level. Local drying protects critical points.
A system can be correctly designed and still drift out of range.
Filters become clogged. Condensate drains fail. Drying media loses performance. Pressure drops increase. Ambient conditions change after a machine is moved or a line is extended.
That is why pressure dew point should not only be treated as a design value. It should also be checked as part of routine compressed air quality monitoring.
Regular checks should include:
These checks help catch moisture risk before it becomes a production problem.
Use this checklist to assess where improvement may be needed:
📘 Download our whitepaper: “Answers to the 5 most frequently asked questions about air prep”
Download nowPressure dew point is a practical way to judge whether compressed air can stay dry under real operating conditions. When the target value matches the application, the environment and the air quality requirement, the system is better protected against condensate, corrosion and unstable performance.