The store will not work correctly when cookies are disabled.
Festo uporablja piškotke za izboljšanje učinkovitosti, optimizacijo funkcionalnosti, analizo dostopov in prilagajanje vsebin in prikazov. Uporabo piškotkov lahko kadar koli prekličete. Dodatne informacije o tem najdete v našem pravilniku o zasebnosti in politiki glede piškotkov.
These include cookies that enable Festo to optimise the website based on users' behaviour (tracking) and are stored anonymously.
These cookies assist users in that optimum suggestions are made based on users' behaviour.
These cookies enhance the functions and convenience of the website. For example, encrypted user data can be stored in them for an automatic logon. These cookies can be stored for a long time.
These cookies are used for enabling the basic function of the Festo website and the online shop. These cookies cannot be deselected.
This software expansion package for the servo press kit YJKP includes force control, an OPC UA connection and the extended sequencer, among other things.