Festo provides a complete system

The dispense head VTOE was the first modular complete solution developed by Festo for quickly and accurately dispensing extremely small quantities of liquids. Festo was thus able to offer customers an integrated system for liquid handling, including kinematics, that is based on the functional principle of pressure over liquid.

By using a proportional pressure regulator, such as the VEAB, pressure is built up in a filled reservoir. The liquid is delivered to a dispense head or a media-separated valve via an additional line. By opening and closing the valve (e.g. VYKA or VYKB) the liquid is dispensed via special fluidic push-in fittings (NLFA) using a dispensing needle (VAVN). The pressure and valve opening time can be used to regulate how much liquid is dispensed. The opening times can be easily adjusted, for example with the valve control module VAEM. Thanks to this setup and a suitable handling system, microwell plates in laboratory automation applications can be precisely filled in no time at all.

New application options

The media-separated solenoid valves VYKA and VYKB and the media-separated pneumatic valve VZDB open up completely new applications beyond those in laboratory automation. These include adding flavorings to food products and feeding ink in the printing industry, cleaning cow teats, controlling fluids in dental chairs and inoculating eggs in the incubation process.

Innovative dispensing solutions and much more

The valve control module VAEM is another LifeTech product that offers very diverse application options. It can switch a wide range of solenoid valves and it makes child’s play of parametrizing all holding current reduction values. This makes it very easy for you to configure your own individual dispensing solution, from a single channel to a 12-channel dispense head and valve control module VAEM.

More effective pipetting

The LifeTech development team in Boston, USA, has developed the new dispense head VTOI which is capable of dispensing to eight outlets via a single inlet. Furthermore, the VTOI can also be used for pipetting, i.e. withdrawing liquids from a particular source and dispensing them elsewhere. All in all, this contributes greatly to further accelerating key processes in laboratory automation. The team in Boston is also working on a complete pipetting system as well as decentralized pressure/vacuum generation. Festo is opening up more and more opportunities and new perspectives to manufacturers for making precision liquid handling even more efficient.