Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

servo drive CMMT-ST-C8-1C-MP-S0 8163946
Description Version
Convert project FCT Convert project

(Servicevideo)

Update firmware (Ethernet) FCT: Update firmware (Ethernet)

(Servicevideo)

Update firmware (USB) FCT Update firmware (USB)

(Servicevideo)

Update plug-in FCT Update plug-in

(Servicevideo)

FSA-202209 - Security Advisory - Incomplete documentation of remote accessible functions and protocols Incomplete documentation of remote accessible functions and protocols in Festo products

Incomplete Festo product documentation of remote accessible functions and their required IP ports. Depending on the product a description of the supported features can be found in the product documentation to some extent.

 

Festo developed the products according to the respective state of the art. As a result, the protocols used no longer fully meet today's security requirements. The products are designed and developed for use in sealed-off (industrial) networks. If the network is not adequately sealed off, unauthorized access to the product can cause damage or malfunctions, particularly Denial of Service (DoS) or loss of integrity.

1.2.1
CMMT AS & CMMT ST Ring Topology MRP with Siemens PLC S7-1500 by Profinet CMMT AS; CMMT ST Ring Topology MRP with Siemens PLC; Profinet; Library included

This Application Note explains how to implement Ring Topology in Festo CMMT-AS and CMMT-ST with Siemens S7-1500 series PLCs over a Profinet in the TIA programming environment. It also describes how to incorporate LPNDR function block library into an TIA programming environment.

1.20
14/05/2024
CMMT EtherCat controlled by C++ CMMT EtherCat controlled by C++; Example project included

This document describes how to control the CMMT EtherCat version with the programming language C++, using the SOEM (Simple Open Source EtherCat Master) library.

1.20
16/09/2025
CMMT Integration with Schneider PLC using Ethernet/IP CMMT-AS; Schneider PLC Integration; Example project included

This Application Note explains the Function Blocks which allows the user to integrate CMMT controller with Schneider PLC and Unity Software using Ethernet/IP

1.10
15/01/2021
CMMT Library for Emerson DeltaV using EtherNet/IP CMMT Library for Emerson DeltaV using EtherNet/IP; Library is included

This application note gives detailed explanation of the library and sample project for Festo Servo Drive CMMT with Emerson DeltaV using EtherNet/IP.

1.20
02/07/2026
CMMT servo drive commissioning MITSUBISHI IQ-R PLC by ETH/IP CMMT-AS; Mitsubisi IQ-R PLC with ETH/IP; Library included

This Application Note gives detailed procedure to integrate CMMT

Servo Drive with Mitsubishi IQ-R Controller in EtherNet/IP communication
network. Also described to Read/Write the servo motor parameter.

1.40
12/08/2024
CMMT Servo Drive Commissioning with ABB Cobot OmniCore Controller through EtherNet/IP CMMT; ABB Cobot OmniCore Controller; Library included

This Application Note Gives Detailed Procedure to Integrate CMMT Servo Drive with ABB Cobot OmniCore Controller in EtherNet/IP Communication Network. Festo_CMMT_Drive library is only for 7th Axis integration.

1.10
12/05/2023
CMMT servo drive commissioning with Allen-Bradley Micro850 PLC through Modbus TCP network .CMMT servo drive; Allen-Bradley Micro850 PLC; Modbus TCP network

This Application Note gives detailed procedures to integrate CMMT Servo Drive with Allen-Bradley Micro850 Controller in Modbus TCP communication Network. It also describes how to control the Servo Motor in different control operational modes.

1.10
25/08/2023
CMMT Servo Drive commissioning with KEBA Controller through EtherCAT CMMT Servo Drive with KEBA Controller through EtherCAT; Library included

This Application Note Gives Detailed Procedure to Integrate CMMT Servo Drive With KEBA Controller using EtherCAT Communication Network. Also Described to Control the Servo Motor in Different Control Operational Modes.

1.10
04/03/2024
CMMT servo drive commissioning with MITSUBISHI FX5U PLC by ETH/IP CMMT-AS; Mitsubisi FX5U with ETH/IP; Library included

This Application Note gives detailed procedure to integrate CMMT

Servo Drive with Mitsubishi FX5U Controller in EtherNet/IP communication
network. Also described to Read/Write the servo motor parameter.

1.40
12/08/2024
CMMT servo drive commissioning with MITSUBISHI PLC by MODBUS TCP CMMT-AS; Mitsubisi FX5U and IQ-R by Modbus TCP; Library included

This Application Note gives detailed procedure to integrate CMMT servo drive with Mitsubishi FX5U and IQ-R controller in MODBUS communication network.

1.20
25/09/2023
CMMT Servo Drive Commissioning with Mitsubishi Q-Series PLC through Modbus TCP CMMT with Mitsubishi Q-Series; GX-Works2; Modbus TCP; Library included

This Application Note gives a step by step description of how to integrate CMMT servo drives from Festo with Mitsubishi Q-Series Controllers over Modbus TCP communication network in GX-Works2 programming environment. It also explains how to integrate the host function block library for CMMT servo drives into a GX-Works2 programming environment and to control the servo motor in different control operational modes.

1.20
08/02/2024
CMMT Servo Drive with Siemens S7-300 PLC by Profinet CMMT Servo Drive with Siemens S7-300 PLC by Profinet; Library included

This application note describes how to use the host function blocks of the CMMT Servo Drives from Festo & integrate them in Siemens SIMATIC Manager with S7-300 PLCs through Profinet network

1.10
08/04/2024
CMMT-AS Servo Drive Commissioning with LS Electric PLC over EtherNet/IP CMMT-AS; CMMT-ST; with LS Electric PLC over EtherNet/IP; Library included

This Application Note gives a step by step description of how to integrate CMMT servo drives from Festo with LS Electric XGT series PLCs over EtherNet/IP network in XG5000 programming environment. It also explains how to integrate the host function block library for CMMT servo drives into a LS Electric XG5000 programming environment.

1.10
07/08/2023
CMMT-AS Servo Drive Commissioning with LS Electric PLC over Modbus TCP CMMT-AS; LS Electric PLC; Modbus TCP

This Application Note explains how to integrate Festo CMMT servo drives with LS Electric XGT series PLCs over a Modbus TCP network in the XG5000 programming environment. It also describes how to incorporate the CMMT servo drive host function block library into an LS Electric XG5000 programming environment.

1.10
22/12/2023
CMMT-AS Servo Drive Control with LS Electric PLC through EtherCAT Network CMMT-AS; CMMT-ST; LS Electric PLC; EtherCAT Network

This application note explains how to control the CMMT-AS servo drive via EtherCAT network in LS Electric PLC. The user will be able to control the Festo drives in point-to-point mode & read/write parameters using the sample code provided.

1.10
17/07/2023
CMMT-AS with Eaton PLC through EtherNetIP CMMT-AS with Eaton PLC through EtherNetIP; Library is included

This Application Note explains how to integrate the CMMT Servo Drive and the function block library for the Festo CMMT Servo Drive through EtherNet/IP with Eaton Controller in XSOFT CODESYS 3 programming environment

1.10
02/07/2025
CMMT-AS-EC controlled by record table with Keyence KV-8000 PLC in KV Studio CMMT-AS-EC with Keyence KV-8000 PLC in KV Studio Example project included

This document describes the commissioning of controlling CMMT-AS-...EC with a KV-8000 PLC & KV-XH16EC EtherCAT module from Keyence in KV Studio.

1.10
26/08/2022
CMMT-AS-MP Position sensor difference monitoring with linear encoder CMMT-AS-MP Position sensor difference monitoring with linear encoder

This Application Note describes how to configure and run the CMMT-AS-MP with servomotor, linear toothed belt axis with 2nd linear encoder to monitor the position difference between the motor encoder 1 [X2] and linear encoder 2 [X3] of the linear toothed belt drive.

1.10
02/01/2025
CMMT-AS-MP Servo Drive Control with Festo CDPX-X-E1-W-xx Operator Panel through Profinet CMMT-AS-MP; Festo CDPX-X-E1-W-xx; Profinet; Sample Code included

This application note explains how to control the CMMT-AS servo drive via Profinet network in Festo CDPX-E operator panels. The user will be able to control the Festo drives in point to-point mode using the sample code provided. The manual refers to the following models CDPX-X-E1-W-7, CDPX-X-E1-W-10 and CDPX-X-E1-W-15.

1.10
11/01/2024
CMMT-AS-PN controlled by Siemens Simotion P320-4 in Siemens Scout 5.3 CMMT-AS; Siemens Scout

This document describes a way to control the CMMT-AS-PN via ProfiDrive protocol 105 with a Simotion P320-4 PLC of Siemens.

1.10
03/03/2020
CMMT-ST-C8-1C-...-S0 with 3rd-party motor and BISS-C Multiturn CMMT-ST, Engel motor, Ever Elettronica motor; Example project included

The FESTO servo drive controller of type CMMT-ST-C8-1C-...-S0 is supporting the encoder feedback system BISS-C with Multiturn.

The following Application Note is a step by step instruction, how to parameterize this system with Festo Automation Suite.

1.10
18/01/2021
CMMT-xx-EP EtherNet/IP Control via MicroLogix1400 PLC CMMT-xx-EP EtherNet/IP; Example project included

This document provides configuration information for the integration of Festo CMMT-xx-EP Drive/Motor Controllers to an  Allen Bradley

MicroLogix1400 PLC.

The control method is EtherNet/IP protocol.

1.10
05/01/2021
CMMT-xx-EP ModbusTCP Server Control via Allen Bradley MicroLogix1400 Client PLC CMMT-xx-EP ModbusTCP Server; Example project included

This document provides configuration information for the integration of Festo CMMT-xx-EP Drive/Motor Controllers (Slave/Server) to an

Allen Bradley MicroLogix1400 PLC (Master/Client).

The control method is ModbusTCP protocol, including PROFIdrive over Modbus.

1.10
05/01/2021
Commissioning Modbus TCP of CMMT-xx-EP in B&R Automation Studio Modbus TCP, CMMT-xx-EP in B&R Automation Studio; Library included

This document describes how to build up a communication over Modbus using FestoPtP library between CMMT-xx-EP and B&R X20 PLC

1.20
20/12/2022
Commissioning of CMMT-AS in Festo Automation Suite with CPX-E-CEC-M1-PN CPX-E-CEC-M1-PN; CMMT-AS-...-EC

This application nodes describes step by step how you

configure a CMMT-AS-EC with CPX-E-CEC-M1-PN in

Automation Suite and how you can use the PTP libraries.

1.10
17/09/2019
Show 26 more results ...