Support Portal

Please select a category on the left or use the search.

Search

Part number

Series

Order code

Description Version
CMMT-AS-MP Position sensor difference monitoring with linear encoder CMMT-AS-MP Position sensor difference monitoring with linear encoder

This Application Note describes how to configure and run the CMMT-AS-MP with servomotor, linear toothed belt axis with 2nd linear encoder to monitor the position difference between the motor encoder 1 [X2] and linear encoder 2 [X3] of the linear toothed belt drive.

1.10
02/01/2025
CMMT-AS-MP Servo Drive Control with Festo CDPX-X-E1-W-xx Operator Panel through Profinet CMMT-AS-MP; Festo CDPX-X-E1-W-xx; Profinet; Sample Code included

This application note explains how to control the CMMT-AS servo drive via Profinet network in Festo CDPX-E operator panels. The user will be able to control the Festo drives in point to-point mode using the sample code provided. The manual refers to the following models CDPX-X-E1-W-7, CDPX-X-E1-W-10 and CDPX-X-E1-W-15.

1.10
11/01/2024
CMMT-AS-PN controlled by Siemens Simotion P320-4 in Siemens Scout 5.3 CMMT-AS; Siemens Scout

This document describes a way to control the CMMT-AS-PN via ProfiDrive protocol 105 with a Simotion P320-4 PLC of Siemens.

1.10
03/03/2020
CMMT-AS-PN controlled by SINAPOS functions block with Siemens S7 1500 controller CMMT-AS-...-PN; Siemens S7 1500; SINAPOS

This document describes which control figures are implemented in CMMT-AS-PN drives and how to use it in programming environment of Siemens in TIA portal. Specifically focus on how to use SINAPOS functions block(PtP non-interpolated motion) in SINAMICS Lib for point to point linear motion.

1.30
27/03/2019
CMMT-AS-PN controlled by technology objects with SIMATIC S7-1500 in the TIA Portal CMMT-AS; Siemens TIA Portal

This document describes which control figures are implemented in CMMT-AS-PN drives and how to use it in programming environment of Siemens in TIA portal. Specifically focus on how to use Technology Objects (Interpolated motion) with PLC Open Function blocks.

1.20
03/12/2020
CMMT-AS-xx with Multiturn Motor and 2nd incremental encoder CMMT-AS, Multiturn Motor and 2nd incremental encoder

This Application Note describes how to configure and run the CMMT-AS-xx with Multiturn Motor and 2nd incremental encoder by using the homing method 'zero pulse'. The 2nd incremental encoder is increasing the absolute accuracy of the linear axis (direct position measurement) and is providing the zero pulse for the homing. The internal multiturn motor encoder gives the possibility to detect the defined and fixed zero pulse for the homing process of the 2nd incremental encoder.
With this strategy we have an accurate reference point and do not need any HWlimit switches, HW-reference switches or any mechanical stops for the needed homing process.

1.10
27/10/2021
CMMT-xx-EP EtherNet/IP Control via MicroLogix1400 PLC CMMT-xx-EP EtherNet/IP; Example project included

This document provides configuration information for the integration of Festo CMMT-xx-EP Drive/Motor Controllers to an  Allen Bradley

MicroLogix1400 PLC.

The control method is EtherNet/IP protocol.

1.10
05/01/2021
CMMT-xx-EP ModbusTCP Server Control via Allen Bradley MicroLogix1400 Client PLC CMMT-xx-EP ModbusTCP Server; Example project included

This document provides configuration information for the integration of Festo CMMT-xx-EP Drive/Motor Controllers (Slave/Server) to an

Allen Bradley MicroLogix1400 PLC (Master/Client).

The control method is ModbusTCP protocol, including PROFIdrive over Modbus.

1.10
05/01/2021
Commissioning Modbus TCP of CMMT-xx-EP in B&R Automation Studio Modbus TCP, CMMT-xx-EP in B&R Automation Studio; Library included

This document describes how to build up a communication over Modbus using FestoPtP library between CMMT-xx-EP and B&R X20 PLC

1.20
20/12/2022
Commissioning of CMMT-AS in Festo Automation Suite with CPX-E-CEC-M1-PN CPX-E-CEC-M1-PN; CMMT-AS-...-EC

This application nodes describes step by step how you

configure a CMMT-AS-EC with CPX-E-CEC-M1-PN in

Automation Suite and how you can use the PTP libraries.

1.10
17/09/2019
Commissioning of CMMT-AS in Festo Automation Suite with CPX-E-CEC-M1-PN CMMT-AS-...-EC; CPX-E-CEC-M1-PN; Example project included

This application note describes step by step how you configure a CMMT-AS-EC with CPX-E-CEC-M1-PN in Automation Suite and how you can use the SoftMotion libraries.

1.10
17/09/2019
Commissioning of CMMT-AS in TwinCAT V3 CMMT-AS; TwinCAT V3

This application nodes describes step by step how you

configure a CMMT-AS-EC in

        • Automation Suite

        • TwinCAT V3

And how you can use the PTP libraries.

1.10
11/10/2018
Commissioning of CMMT-AS-PN in B&R Automation Studio Commissioning of CMMT-AS-PN in B&R-PLC; Example project included

This short Application Note shows how to establish a Profinet communication between a B&R-PLC and a CMMT-AS-…-PN.

1.10
28/01/2021
Configuration of CMMT-AS-EC(PN) to run 3rd party motor CMMT-AS-...EC

This document describes how to configure and run 3rd party motors in combination with CMMT-AS-..-EC (PN) drive.

1.20
23/01/2019
Conversion of CMMT-EC/PN/EP to Multi Protocol Conversion of CMMT-EC/PN/EP to MP

This document explains how to convert existing applications
that use CMMT-AS-x-EC/PN/EP-x to CMMT-AS-x-MP-x

1.10
20/05/2022
Device service and methods in CMMT-xx-MP executing and resetting via Siemens PLC TIA environment Device service and Methods, CMMT-xx-MP, Siemens TIA

This application note describes the using of the device services and methods offered for certain functions in CMMT-XX-MP within the TIA environment controlled by a Siemens PLC.

1.10
21/03/2023
EMC - Checklist General

A checklist to avoid EMC trouble

 

1.10
03/03/2023
Festo CMMT-AS Servo Drive Commissioning with Keyence PLC through EtherNet/IP Network CMMT-AS; Keyence KV 7000 and KV 8000 Series; EtherNet/IP; Library included

This application note gives detailed explanation of the host function blocks of CMMT-AS Servo Drive which allows user to integrate & control CMMT-AS controller with Keyence KV-8000 and KV-7000 PLC using EtherNet/IP protocol.

1.20
12/12/2023
Festo CPX-AP-.-EC with B&R PLC through EtherCAT Festo CPX-AP-.-EC with B&R PLC through EtherCAT; Library included

This Application Note gives a step by step description of how to integrate Festo CPX-AP-.-EC EtherCAT interface with B&R PLC in Automation Studio programming environment. This library is intended for common use of CPX-AP-I-EC and CPX-AP-A-EC.

1.10
10/04/2025
Festo Motion Package - User Guide Festo Motion Package - User Guide

A guide to commission and program single axis using Festo Motion Package in Festo edge controller CEPE. Drive used is a CMMT-AS-C2-3A-MP-S1.

Other quick start guide shows the steps to get an example system working with Festo Robotic as part of Festo Motion Package. In the end user will be able to start programming his own application.

1.40
14/10/2026
Festo Positioning CNC Robotics Library (FPosCR Lib) V3.5.18.50 (EVO2.1) Festo Positioning CNC Robotics Library (FPosCR Lib) V3.5.18.50 (EVO2.1); Library is included

Festo Positioning CNC Robotics Library provides CNC and robotic motion functionalities for Festo gantry systems.

1.20
06/03/2026
How to connect CMMT through EtherCat to an OMRON PLC in Sysmac Studio CMMT; NJ301-1100 Omron PLC; Example Project included

This document will go through a Step by Step description of what must be done to connect CMMT to an OMRON PLC through EtherCAT and integrating it to the Motrion Control (MC) ele-ments

1.40
15/02/2022
How to connect CMMT to a BECKHOFF IPC in TwinCAT V3 NC CMMT, TwinCAT V3

Step by step description of how to start a project in TwinCAT V3 and what needs to be done to integrate CMMT into the NC ele-ment

1.10
02/04/2025
How to connect CMMT to a BOSCH ctrlX-OS How to connect CMMT to a BOSCH ctrlX-OS

Step by step description of how to start a project in BOSCH ctrlX-OS and what needs to be done to integrate CMMT into the motion control element

1.10
22/01/2026
How to connect CMMT to an OMRON PLC in Sysmac Studio via Ethernet/IP CMMT-AS/ST OMRON PLC in Sysmac Studio via Ethernet IP; Example project included

This document will go through a Step by Step description of what must be done to connect CMMT to an OMRON PLC through Ethernet/IP and how to control via ProfiDrive.

1.10
07/12/2022
How to setup „Travel to fixed stop“ with CMMT-AS-PN by using the SINA_POS / telegram 111 CMMT-AS-...PN

This document describes how to set up the CMMT-AS-...-PN in "trav-el to fixed stop" mode by using the SINA_POS function block / telegram 111 in programming environment of TIA Portal

1.30
10/04/2025
Implementing SLS-Safety function based on CMMT-AS X2/X3 encoder evaluation and X10 encoder emulation CMMT-AS-...-S1 CMMT-AS-...-S1

Implementing SLS-Safety function based on CMMT-AS X2/X3 encoder evaluation and X10 encoder emulation CMMT-AS-...-S1

1.10
25/09/2020
Information on substances in our products Substances in our products; Compliance

Festo SE & Co KG complies with national and international laws, guidelines, standards and regulations which are applicable to our products. We constantly monitor the dynamics of legislation. This Application Note give an overview.

V3.5
17/10/2026
Input Shaping Vibration Compensation with servo drives CMMT-AS and CMMT-ST Input Shaping Vibration Compensation with servo drives CMMT-AS and CMMT-ST

Brief description and practical example of setting and handling the Vibration Compensation with the servo drive controllers CMMT-AS and CMMT-ST using the Festo Automation Suite (FAS)

1.10
06/12/2023
Release Notes CMMT-AS-MP Release Notes CMMT-AS-MP

1     New Features in Version 36.10.4. 2

2     Fixed Bugs in Version 36.10.4. 3

3     New Features in Version 36.10.3. 4

4     Fixed Bugs in Version 36.10.3. 5

5     New Features in Version 35.9.2 (V352) 7

6     Fixed Bugs in Version 35.9.2 (V352) 8

09/02/2026
Show 10 more results ...
When searching, you can get detailed product information (e.g. CAD support and technical data) with part no. or order code.
If they are not available, use the Product selection in the catalogue.